SLUUC21A July   2019  – July 2021 TPS62866

 

  1. 1Introduction
    1. 1.1 Performance Specification
    2. 1.2 Modifications
  2. 2Setup
    1. 2.1 Input/Output Connector Descriptions
    2. 2.2 Setup
  3. 3TPS62866EVM-051 Test Results
  4. 4Board Layout
  5. 5Schematic and List of Materials
    1. 5.1 Schematic
    2. 5.2 List of Materials
  6. 6Software User Interface
    1. 6.1 Software Setup
    2. 6.2 Interface Hardware Setup
    3. 6.3 User Interface Operation
      1. 6.3.1 Home Screen
      2. 6.3.2 Settings Screen
      3. 6.3.3 Register Map Screen
  7. 7Revision History

Input/Output Connector Descriptions

    J1, Pin 1 and 2 – VIN Positive input connection from the input supply for the EVM
    J1, Pin 3 and 4 – S+/S- Input voltage sense connections. Measure the input voltage at this point.
    J1, Pin 5 and 6 – GND Input return connection from the input supply for the EVM
    J2, Pin 1 and 2 – VOUT Output voltage connection
    J2, Pin 3 and 4 – S+/S- Output voltage sense connections. Measure the output voltage at this point.
    J2, Pin 5 and 6 – GND Output return connection
    J3, Pin 5 – VBUS The VBUS pin of this header is used to bias the SCL and SDA nodes of I²C interface via a resistor.
    J3, Pin 6 – GND The GND pin of this header is used to connect the grounds of the IC and the I²C interface.
    J3, Pin 9 – SCL The pin of this header should be connected to the SCL of the I²C interface.
    J3, Pin 10 – SDA The pin of this header should be connected to the SDA of the I²C interface.
    JP1 – VID/PG VID/ PG pin jumper. Always place the jumper across VID/ PG and LOW pins before start-up. This sets the output voltage and device address. After startup, VOUT reflects the value set on VOUT Register 1 if the jumper is placed across VID/ PG and LOW pins. VOUT follows the value set on VOUT Register 2 if the jumper is placed across VID/ PG and HIGH pins.
    JP2 – EN EN pin input jumper. Place the jumper across ON and EN to turn on the IC. Place the jumper across OFF and EN to turn off the IC.