SLUUC21A July 2019 – July 2021
Upon start-up, the GUI automatically connects to the EVM. If not, then click on the "Connect" button in the lower-left corner of the GUI window. Ensure the I2C Slave Address is correct. The following sections give a short overview of the three main GUI screens.