SLAA701B October 2016 – June 2026 TAS5342A , TAS5342LA , TAS5352 , TAS5630B , TPA3220 , TPA3221 , TPA3251 , TPA3255 , TPA3255-Q1
Since the Cg capacitors on the Type-2 filter share a common node through ground, differential signals will see a capacitance value of Cg / 2 since the capacitors appear in series for differential signals only. Therefore, with proper selection of the Cg capacitance value, the Type-2 can also be used for AD modulation class-D amplifiers which require a differential filter. Conversion from Type-1 to Type-2 only requires scaling of CBTL by a factor of 2. That is, Cg = 2 x CBTL for identical filter cut-off frequency and damping factor.
Figure 1-19 Type-1 AD Modulation Filter Converted to Type-2