SFFSA43A December   2024  – September 2025 LM5125-Q1 , LM5125A-Q1

 

  1.   1
  2.   Trademarks
  3. 1Overview
  4. 2Functional Safety Failure In Time (FIT) Rates
    1. 2.1 VQFN Package
  5. 3Failure Mode Distribution (FMD)
  6. 4Pin Failure Mode Analysis (Pin FMA)
    1. 4.1 LM5125-Q1 (VQFN) Package
    2. 4.2 LM5125A-Q1 (VQFN) Package
    3. 4.3 LM51251A-Q1 (VQFN) Package
  7. 5Revision History

LM51251A-Q1 (VQFN) Package

Figure 4-2 shows the LM51251A-Q1 pin diagram for the VQFN package. For a detailed description of the device pins, see the Pin Configuration and Functions section in the LM51251A-Q1 data sheet.

Figure 4-3 Pin Diagram (VQFN) Package
Table 4-10 Pin FMA for Device Pins Short-Circuited to Ground
Pin Name Pin No. Description of Potential Failure Effects Failure Effect Class
DLY 1 The average-input-current loop is not activated when the average-input-current loop feature is used. B
D
SS 2 The device does not start; no switching. B
COMP 3 VOUT is out of regulation; not switching. B
AGND 4 No effect. D
CSN1 5 The device is potentially damaged if the differential voltage exceeds the absolute maximum rating of 0.3V. A
CSP1 6 The device is potentially damaged if the differential voltage exceeds the absolute maximum rating of 0.3V. A
VOUT 7 The external components are potentially damaged. The device potentially goes into a latch state or does not start. B
HO1 8 The phase-1 high-side driver is potentially damaged when the device starts switching. A
HB1 9 The device is potentially damaged when BOOT charging starts. A
SW1 10 No energy is transferred from the input to the output. B
LO1 11 The phase-1 low-side driver is potentially damaged when the device starts switching. A
VCC 12 There is a loss of VCC regulation; no switching. B
PGND 13 No effect. D
LO2 14 The phase-1 low-side driver is potentially damaged when the device starts switching. A
SW2 15 No energy is transferred from the input to the output. B
HB2 16 The device is potentially damaged when BOOT charging starts. A
HO2 17 The phase-2 high-side driver is potentially damaged when the device starts switching. A
BIAS 18 The device is not powered, and therefore, not functional. B
UVLO/EN 19 The device is disabled. B
CSP2 20 The device is potentially damaged if the differential voltage exceeds the absolute maximum rating of 0.3V. A
CSN2 21 The device is potentially damaged if the differential voltage exceeds the absolute maximum rating of 0.3V. A
RT 22 The device goes to the maximum switching frequency of >2.2MHz. C
SYNCOUT 23 The device is potentially damaged if the device configuration has the SYNCOUT function enabled. A
D
SYNCIN 24 Clock synchronization is disabled; the device uses the internal clock. C
SDA 25 I2C communication does not work. B
SCL 26 I2C communication does not work. B
CFG 27 Level 1 of the CFG pin is forced. C
nFAULT 28 The voltage of the output is correct, but there is a loss of functionality at the nFAULT pin. B
MODE 29 Diode emulation mode is activated. There is no effect if the device is configured for diode emulation mode (MODE = GND). C
D
EN2 30 Second phase is disabled if second phase is used. C
D
ILIM/IMON 31 The average-input-current loop is not activated; current monitoring does not work. B
ATRK/DTRK 32 There is no output voltage regulation. The device enters BYPASS mode after the soft start completes. B
Table 4-11 Pin FMA for Device Pins Open-Circuited
Pin Name Pin No. Description of Potential Failure Effects Failure Effect Class
DLY 1 Delayed programming does not work if the delay pin function is used. B
D
SS 2 There is a short soft-start time. C
COMP 3 The device is potentially unstable. B
AGND 4 Device damage is possible. A
CSN1 5 There is a loss of the current sense signal for phase 1. Peak-current limit does not work. B
CSP1 6 There is a loss of the current sense signal for phase 1. Peak-current limit does not work. B
VOUT 7 The internal feedback voltage for the regulation loop is pulled to GND; VOUT reaches OVPmax. B
HO1 8 There is a loss of the high-side driver. B
HB1 9 There is a loss of boot voltage, and hence, a loss of the high-side driver. B
SW1 10 There is a loss of the high-side driver. B
LO1 11 The low-side MOSFET does not switch for phase 1. B
VCC 12 The VCC pin is not stable enough to sustain normal operation. B
PGND 13 Device damage is possible. A
LO2 14 The low-side MOSFET does not switch for phase 2. B
SW2 15 There is a loss of the high-side driver. B
HB2 16 There is a loss of boot voltage, and hence, a loss of the high-side driver. B
HO2 17 There is a loss of the high-side driver. B
BIAS 18 The device is not powered, and therefore, not functional. B
UVLO/EN 19 The device is disabled. B
CSP2 20 There is a loss of the current sense signal for phase 2. Peak-current limit does not work. B
CSN2 21 There is a loss of the current sense signal for phase 2. Peak-current limit does not work. B
RT 22 The minimum frequency is set. C
SYNCOUT 23 The primary device functions normally. The secondary device does not get a switching clock in a multi-device configuration. C
B
SYNCIN 24 Clock synchronization does not work; the device uses the internal clock. C
SDA 25 I2C communication does not work. B
SCL 26 I2C communication does not work. B
CFG 27 Level 16 of the CFG pin is forced. C
nFAULT 28 The output voltage is correct, but there is a loss of functionality at the nFAULT pin. B
MODE 29 There is no effect if DEM mode is active, otherwise, DEM mode is activated. D
C
EN2 30 Second-phase enable potentially does not function as intended. C
ILIM/IMON 31 The device operates in an average-input-current limit loop operation; VOUT drops, and therefore, VOUT is out of regulation. B
ATRK/DTRK 32 The device goes to OVPmax. B
Table 4-12 Pin FMA for Device Pins Short-Circuited to Adjacent Pin
Pin Name Pin No. Shorted to Description of Potential Failure Effects Failure Effect Class
DLY 1 SS There is a loss of the delay function; the average-input-current loop does not function as intended. B
SS 2 COMP The device operates in peak-current limit and the output voltage rises to OVPmax. B
COMP 3 AGND The VOUT regulation loop does not function, the internal supply potentially collapses. B
AGND 4 CSN1 The device is potentially damaged if the differential voltage exceeds the absolute maximum rating of 0.3V. A
CSN1 5 CSP1 There is a loss of current sense information. The circuit is potentially unstable. B
CSP1 6 VOUT The output is shorted to the input supply. There is no output regulation. B
VOUT 7 HO1 Device damage is possible as the HO1 pin exceeds the absolute maximum voltage rating to switch. A
HO1 8 HB1 Device damage is possible when switching starts. A
HB1 9 SW1 There is a loss of the high-side driver. B
SW1 10 LO1 Device damage is possible as the absolute maximum rating is exceeded at the LO1 pin. A
LO1 11 VCC The LO1 pin does not switch. Device damage is possible when switching starts. A
VCC 12 PGND There is no VCC rail; no switching. B
PGND 13 LO2 Device damaged is possible when switching starts. A
LO2 14 SW2 Device damage is possible as the absolute maximum rating is exceeded at the LO2 pin. A
SW2 15 HB2 There is a loss of the high-side driver. B
HB2 16 HO2 Device damage is possible when switching starts. A
HO2 17 BIAS Device damage is possible as the HO2 pin potentially exceeds the absolute maximum voltage ratings at the pin locations of HO2 to SW2. A
BIAS 18 UVLO/EN There is a loss of the UVLO function; the device is always enabled. B
C
UVLO/EN 19 CSP2 There is incorrect current sense information, the current limit is potentially incorrect. B
CSP2 20 CSN2 There is a loss of current sense information. The circuit is potentially unstable. B
CSN2 21 RT Device damage is possible. The CSN2 pin exceeds the absolute maximum voltage rating for the RT pin. A
RT 22 SYNCOUT The device operates at the maximum switching frequency at start-up. When the SYNCOUT pin starts switching, switching is unstable. C
SYNCOUT 23 SYNCIN There is a loss of the frequency synchronization function; switching frequency is unstable. B
SYNCIN 24 SDA I2C communication does not working when an external clock is used or the SYNCIN pin is connected to GND. I2C operates normally when the SYNCIN pin is left floating. The device potentially synchronizes to the SDA signal when clock synchronization is enabled. There is a loss of the frequency synchronization function. B
SDA 25 SCL I2C communication does not work. B
SCL 26 CFG I2C communication does not work for the device if the resistance of the CFG pin is strong enough to pull down the I2C clock. The device configuration for the CFG pin is incorrect. B
CFG 27 nFAULT The device loses the function of the configuration. B
nFAULT 28 MODE The MODE function of the device is effected. The device potentially functions in an operation mode that is incorrect based on the nFAULT output. C
MODE 29 EN2 The incorrect operation MODE or phase 2 enables or disables incorrectly depending on the voltage that is driven. B
EN2 30 ILIM/IMON The device is forced to function in average-input-current limit mode if the EN2 pin is driven high. The function of the ILIM/IMON pin is lost if the EN2 pin is driven low. B
ILIM/IMON 31 ATRK/DTRK The voltage of the output is not regulated to target the intended value, and the function of the IMON/ILIM pin is lost. B
ATRK/DTRK 32 DLY The voltage of the output is not regulated to target the intended value. The average-input-current limit does not work as intended. B
Table 4-13 Pin FMA for Device Pins Short-Circuited to VI
Pin Name Pin No. Description of Potential Failure Effects Failure Effect Class
DLY 1 Device damage is possible; exceeds the absolute maximum voltage rating. A
SS 2 Device damage is possible; exceeds the absolute maximum voltage rating. A
COMP 3 Device damage is possible; exceeds the absolute maximum voltage rating. A
AGND 4 Device damage is possible; exceeds the absolute maximum voltage rating. A
CSN1 5 There is a loss of the current sense signal. The circuit is potentially unstable. B
CSP1 6 Normal operation. D
VOUT 7 There is a loss of VOUT regulation as the output voltage is forced to VI. B
HO1 8 Device damage is possible as the HO1 pin potentially exceeds the absolute maximum voltage ratings at the pin locations of HO1 to SW1. A
HB1 9 Device damage is possible as the HB1 pin exceeds the absolute maximum voltage ratings at the pin locations of HB1 to SW1. A
SW1 10 Energy is not transferred from input to output. B
LO1 11 Device damage is possible; exceeds the absolute maximum voltage rating. A
VCC 12 Device damage is possible; exceeds the absolute maximum voltage rating. A
PGND 13 Device damage is possible. A
LO2 14 Device damage is possible; exceeds the absolute maximum voltage rating. A
SW2 15 Energy is not transferred from input to output. B
HB2 16 Device damage is possible as the HB2 pin potentially exceeds the absolute maximum voltage ratings at the pin locations of HB2 to SW2. A
HO2 17 Device damage is possible as the HO2 pin potentially exceeds the absolute maximum voltage ratings at the pin locations of HO2 to SW2. A
BIAS 18 Normal operation. D
UVLO/EN 19 No UVLO functionality, the device is enabled or disabled with VI. B
C
CSP2 20 Normal operation. D
CSN2 21 There is a loss of the current sense signal. The circuit is potentially unstable. B
RT 22 Device damage is possible; exceeds the absolute maximum voltage rating. A
SYNCOUT 23 The device is potentially damaged; exceeds the absolute maximum voltage rating. A
SYNCIN 24 Device damage is possible; exceeds the absolute maximum voltage rating. A
SDA 25 Device damage is possible; exceeds the absolute maximum voltage rating. A
SCL 26 Device damage is possible; exceeds the absolute maximum voltage rating. A
CFG 27 Device damage is possible; exceeds the absolute maximum voltage rating. A
nFAULT 28 Device damage is possible; exceeds the absolute maximum voltage rating. A
MODE 29 Device damage is possible; exceeds the absolute maximum voltage rating. A
EN2 30 Device damage is possible; exceeds the absolute maximum voltage rating. A
ILIM/IMON 31 Device damage is possible; exceeds the absolute maximum voltage rating. A
ATRK/DTRK 32 Device damage is possible; exceeds the absolute maximum voltage rating. A