SDAA295 March 2026 DS90LV012A
To properly decode AUX channel signals, the hardware must be implemented correctly. More specifically, AUX polarities must be matched between EVM and the AUX channels. With properly matched AUX polarities, each AUX transaction includes both a SYNC END/START and STOP sequence as depicted in Figure 4-3. Conversely, a hardware implementation with swapped AUX polarities does not have a SYNC END/START or STOP sequence as shown in Figure 4-4.
Figure 4-3 Proper Polarities AUX Transaction
Figure 4-4 Swapped Polarities AUX TransactionIf AUX polarities are found to be incorrect, swap the AUX+ and AUX- wires on the DS90LV011-12AEVM.
Upon capturing the AUX channel, using a dedicated AUX analyzer extension enables efficient parsing of captured signals. Figure 4-5 shows the AUX waveform decoded by utilizing this AUX analyzer extension, which can be applied to the Logic 2 analyzer.
Figure 4-5 Logic 2 AUX Waveform Utilizing AUX Analyzer ExtensionWhen using Logic 2 software, place the AUX analyzer extension in the Logic\resources\windows-x64\Analyzers folder, as shown in Figure 4-6.
Figure 4-6 AUX Analyzer Extension in Logic 2 SoftwareTo apply the extension on Logic 2, follow these steps:
Figure 4-7 Steps to Apply AUX Extension on Logic 2When using the AUX Analyzer extension, make sure the sampling rate is at least 250MS/s.