SDAA265 April 2026 TPS26750A
Changed fields from the default values for this example:
| NoCapabilityMismatch | AutoDisableSinkUponCapabilityMismatch | Sink Path Effects |
|---|---|---|
| 0 | 0 | Request PDO asserts Capability Mismatch but sink path is still enabled regardless of ANSinkCapMismatchPower. |
| 0 | 0 | Request PDO asserts Capability Mismatch and sink path disabled when PDO Power < ANSinkCapMismatchPower |
| 1 | 0 | Request PDO does NOT assert Capability Mismatch. AutoDisableSinkUponCapabilityMismatch ignored |
| 1 | 1 | Request PDO does NOT assert Capability Mismatch. AutoDisableSinkUponCapabilityMismatch ignored |
Figure 3-3 Capability Mismatch is
asserted in the Request Message causing PD device to not enable the
PPHV_EN
Figure 3-4 Request Data Object from the
PD Device to the PD Source.
The Capability mismatch flag is set here which causes the PD Device to NOT enable the PPHV_EN above.
If the system can still be powered at less than the AUTO_NEGOTIATE_SINK.ANSinkCapMismatchPower value, then set AUTO_NEGOTIATE_SINK.NoCapabilityMismatch to 0 or 1 depending on if system needs to assert Capability Mismatch in the Request PDO. And AUTO_NEGOTIATE_SINK.AutoDisableSinkUponCapabilityMismatch to 0.
Figure 3-5 Capability Mismatch is
asserted in the Request Message but PD device still enables PPHV_EN
Figure 3-6 Request Data Object from the
PD Device to the PD Source
Figure 3-7 Capability Mismatch is not
asserted in the Request Message
Figure 3-8 Request Data Object from the
PD Device to the PD Source