SDAA265 April 2026 TPS26750A
If the system can always handle the largest voltage in SPR (up to 20V) or EPR (up to 48V) then leaving AUTO_NEGOTIATE_SINK.AutoComputeSinkMaxVoltage = 1 is acceptable. This means PD looks at the source PDOs offered and set this value to the maximum voltage value.
If the system requires a specific maximum and cannot exceed the voltage, then setting AUTO_NEGOTIATE_SINK.AutoComputeSinkMaxVoltage = 0 means the AUTO_NEGOTIATE_SINK.AutoNegMaxVoltage is set by configuration or by the EC regardless of the source PDO voltages.
(Show test 4 with PD setting MaxVoltage
Figure 3-9 PD Device auto computes
AUTO_NEGOTIATE_SINK.AutoNegMaxVoltage
Figure 3-10 PD Device Always Requesting
15V PDO
Figure 3-11 USB-PD Capture of the 20V PDO
Offered