SDAA161 December 2025 TMS320F280025C , TMS320F280037C , TMS320F280039C , TMS320F280041C , TMS320F280049C , TMS320F28379D , TMS320F28379S , TMS320F28P550SG , TMS320F28P550SJ , TMS320F28P650DH , TMS320F28P650DK , TMS320F28P650SH , TMS320F28P650SK
The design has been validated with the LaunchPad LAUNCHXL-F280039C, and Kingst Logic Analyzer, as shown in Figure 4-1.
Figure 4-1 Test Platform SetupFigure 4-2 shows the test results during positive cycle, where EPWM5A starts CBC protection right at the fault event, while EPWM1B turns low after a delay of 2.098us measured, with 2us setting in CLB. The actual delay is a bit longer than the defined value due to the inherent delay with CLB hardware logic circuits. Figure 4-3 shows the fault event during a negative cycle, where the delayed protection logic also works as expected.
Figure 4-2 Fault Active Low During Positive
Cycle
Figure 4-3 Fault Active Low During Negative
Cycle