SBOK045 March 2024 INA901-SP
The INA901-SP is packaged in a 8-pin HKX package.Figure 3-1 shows the pinout diagram. The evaluation board used for the SEE characterization is shown in Figure 3-2 and schematics are shown in Figure 3-3. During the testing, the LM193AJRLQMLV device was not populated on the EVM.
Note that the package was delidded to reveal the die face for all heavy-ion testing.
Figure 3-1 INA901-SP Pinout
Figure 3-3 INA901-SP Evaluation Board
Schematic