SBAU433B November 2025 – April 2026 ADS125H18
Figure 2-2 shows the schematic for one input channel that, by default, measures differential voltage signals from -10V to +10V. This voltage is measured directly by the ADS125H18 without the need for external attenuation. Table 2-6 describes the function of each component in the differential voltage input channel schematic. Additionally, Table 2-6 references component designators specifically from Figure 2-2; however, the information in the table generally applies to all differential voltage input channels.
COMPONENT | FUNCTION |
|---|---|
Terminal block (17) | Apply one differential voltage signal per terminal block |
| TVS diode (U19 and U20) |
The TVS diodes are not installed by default on this channel |
Shunt (R51) | Converts the current signal to a voltage to be read by the ADC The shunt is not installed by default on this channel |
Zener diodes (D16 and D18) | Protection device that limits the current through the shunt in case of a sustained positive or negative overvoltage event The Zener diodes are not installed by default on this channel |
| 0Ω resistor (R54) | Placeholder for a PTC fuse that must only be installed when the user reconfigures this channel for differential current measurements |
Filter components (R48, R49, C41, C47, and C48) | Provides additional input filtering if desired The capacitors are not installed by default on this channel. The installed resistors are 0Ω |
Figure 2-2 shows that the default voltage input channel configuration is differential-ended. As a result, the EVM supports measurement of voltage inputs that are at different common-mode voltages. However, verify that the absolute voltage on any input pin does not exceed the values specified in the ADS125H18 datasheet.
A differential voltage input channel can also be configured as a differential current input channel by installing the PCB-mounted shunt and Zener diodes, as well as replacing the 0Ω resistor with a PTC fuse.