SBAU361 December 2020
The following equipment is included in the EVM evaluation kit:
The following equipment is not included in the EVM evaluation kit, but is required for evaluation of this EVM:
TI recommends the following generators:
A bandpass filter is required for the analog input signal due to most signal generators addition of phase noise or spurious components. A bandpass filter should also be used for the sample clock input. The DCLKIN input does not require a bandpass filter. If bandpass filters are not used, then the true performance of the ADC may not be seen clearly, and will be limited by the performance of the signal generators being used.
The following recommended bandpass filter will have: