ZHCSAA3B September 2012 – September 2015 TPA3112D1-Q1
PRODUCTION DATA.
The TPA3112D1-Q1 is AEC-Q100 qualified with a temperature grade 1 (-40°C to 125°C), HBM ESD classification level H2, and CDM ESD classification level C2. This automotive audio amplifier also features several protection mechanisms.
The TPA3112D1-Q1 has circuitry that protects the speakers from DC current which might occur due to defective capacitors on the input or shorts on the printed circuit board at the inputs. A DC detect fault is reported on the FAULT pin as a low state. The DC detect fault also causes the amplifier to shut down by changing the state of the outputs to Hi-Z. To clear the DC detect it is necessary to cycle the PVCC supply. Cycling SD does NOT clear a DC detect fault.
A DC detect fault is issued when the output differential duty-cycle exceeds 14% (for example, 57%, –43%) for more than 420 ms at the same polarity. This feature protects the speaker from large DC currents or AC currents, less than 2 Hz. To avoid nuisance faults due to the DC detect circuit, hold the SD pin low at power-up until the signals at the inputs are stable. Also, take care to match the impedance seen at the positive and negative input to avoid nuisance DC detect faults.
The minimum differential input voltages required to trigger the DC detect are shown in Table Table 1. The inputs must remain at or above the voltage listed in the table for more than 420 ms to trigger the DC detect.
| AV (dB) | VIN (mV, Differential) |
|---|---|
| 20 | 112 |
| 26 | 56 |
| 32 | 28 |
| 36 | 17 |
TPA3112D2 has protection from overcurrent conditions caused by a short circuit on the output stage. The short circuit protection fault is reported on the FAULT pin as a low state. The amplifier outputs are switched to a Hi-Z state when the short circuit protection latch is engaged. The latch can be cleared by cycling the SD pin through the low state.
If automatic recovery from the short circuit protection latch is desired, connect the FAULT pin directly to the SD pin. This allows the FAULT pin function to automatically drive the SD pin low which clears the short circuit protection latch.
Thermal protection on the TPA3112D1-Q1 prevents damage to the device when the internal die temperature exceeds 150°C. There is a ±15°C tolerance on this trip point from device to device. Once the die temperature exceeds the thermal set point, the device enters into the shutdown state and the outputs are disabled. This is not a latched fault. The thermal fault is cleared once the temperature of the die is reduced by 15°C. The device begins normal operation at this point with no external system interaction.
Thermal protection faults are NOT reported on the FAULT terminal.
The GVDD supply is used to power the gates of the output full bridge transistors. It can also used to supply the PLIMIT voltage divider circuit. Add a 1-μF capacitor to ground at this pin.
The gain of the TPA3112D1-Q1 is set to one of four options by the state of the GAIN0 and GAIN1 pins. Changing the gain setting also changes the input impedance of the TPA3112D1-Q1.
Refer to Table 2 for a list of the gain settings.
| GAIN1 | GAIN0 | AMPLIFIER GAIN (dB) | INPUT IMPEDANCE (kΩ) |
|---|---|---|---|
| TYP | TYP | ||
| 0 | 0 | 20 | 60 |
| 0 | 1 | 26 | 30 |
| 1 | 0 | 32 | 15 |
| 1 | 1 | 36 | 9 |
The SD pin can be used to enter the shutdown mode which mutes the amplifier and causes the TPA3112D1-Q1 to enter a low-current state. This mode can also be triggered to improve power-off pop performance.
The PLIMIT pin limits the output peak-to-peak voltage based on the voltage supplied to the PLIMIT pin. The peak output voltage is limited to four times the voltage at the PLIMIT pin.
Figure 15. Plimit Circuit Operation
The PLIMIT circuits sets a limit on the output peak-to-peak voltage. The limiting is done by limiting the duty cycle to fixed maximum value. This limit can be thought of as a virtual voltage rail which is lower than the supply connected to PVCC. This virtual rail is four times the voltage at the PLIMIT pin. This output voltage can be used to calculate the maximum output power for a given maximum input voltage and speaker impedance.
Where:
RS is the total series resistance including RDS(on), and any resistance in the output filter.
RL is the load resistance.
VP is the peak amplitude of the output possible within the supply rail.
VP = 4 × PLIMIT voltage if PLIMIT < 4 × VP
POUT(10%THD) = 1.25 × POUT(unclipped)
| TEST CONDITIONS | PLIMIT VOLTAGE (V) | OUTPUT POWER (W) | OUTPUT VOLTAGE AMPLITUDE (VP-P) |
|---|---|---|---|
| PVCC = 24 V, VIN = 1 VRMS, RL = 4 Ω, Gain = 20 dB |
6.97 | 22.1 | 26.9 |
| PVCC = 24 V, VIN = 1 VRMS, RL = 4 Ω, Gain = 20 dB |
1.92 | 10 | 15 |
| PVCC = 24 V, VIN = 1 VRMS, RL = 4 Ω, Gain = 20 dB |
1.24 | 5 | 10 |
| PVCC = 12 V, VIN = 1 VRMS, RL = 4 Ω, Gain = 20 dB |
6.95 | 17.2 | 20.9 |
| PVCC = 12 V, VIN = 1 VRMS, RL = 4 Ω, Gain = 20 dB |
1.75 | 10 | 15.3 |
| PVCC = 12 V, VIN = 1 VRMS, RL = 4 Ω, Gain = 20 dB |
1.2 | 5 | 10.3 |