ZHCSMW9B October 2021 – April 2024 DLP800RE
PRODUCTION DATA
The DMD features a built-in thermal diode that measures the temperature at one corner of the die outside the micromirror array. The thermal diode can be interfaced with the TMP411 temperature sensor as shown in Figure 7-4. The software application contains functions to configure the TMP411 to read the DLP800RE DMD temperature sensor diode. This data can be leveraged by the customer to incorporate additional functionality in the overall system design such as adjusting illumination, fan speeds, etc. All communication between the TMP411 and the DLPC4430 display controller happens over the I2C interface. The TMP411 connects to the DMD through pins outlined in Section 4.
Leave TEMP_N and TEMP_P pins unconnected (NC) if the temp sensor is not used.