ZHCSO96B June 2021 – June 2022 DAC12DL3200
PRODUCTION DATA
The sine wave generation produces full-scale positive values that are one LSB higher than can be represented by the DAC output. In addition, ~1/2 LSB of dither is added to the signal before rounding. Thus setting NCO_GAIN_A or NCO_GAIN_B to values below 0x0003 results in clipping for some frequencies. This range also needs to be taken into account when summing the two NCOs.
When TXENABLE transitions low, the output of the NCO is linearly scaled to zero in a programmable number of clocks set by NCO_RAMPRATE. The same setting is used when TXENABLE transition high.