ZHCSHY1 March 2018 CSD86356Q5D
PRODUCTION DATA.
The power block has the ability to utilize the GND planes as the primary thermal path. As such, the use of thermal vias is an effective way to pull away heat from the device and into the system board. Concerns of solder voids and manufacturability problems can be addressed by the use of three basic tactics to minimize the amount of solder attach that will wick down the via barrel:
In the end, the number and drill size of the thermal vias should align with the end user’s PCB design rules and manufacturing capabilities.
Figure 33. Recommended PCB Layout (Top Down View)
Figure 34. Recommended PCB Layout (Bottom View) (1)