ZHCSOK7B March 2020 – May 2021 CC3130
PRODUCTION DATA
The 3-wire UART topology requires only the following lines (see Figure 8-20):
Using this topology requires meeting one of the following conditions:
Because there is no full flow control, the host cannot stop the SimpleLink™ device to send its data; thus, the following parameters must be carefully considered: