ZHCSFX3A April 2016 – November 2016 CC2564C
PRODUCTION DATA.
The CC2564C architecture comprises a DRP and a point-to-multipoint baseband core. The architecture is based on a single-processor ARM7TDMI® core. The device includes several on-chip peripherals to enable easy communication with a host system and the Bluetooth BR, EDR, and low energy core.
NOTE:
The following technologies and assisted modes cannot be used simultaneously with the coprocessor: Bluetooth low energy, assisted HFP 1.6 (WBS), and assisted A2DP. Only one technology or assisted mode can be used at a time.This section describes the available clock inputs. For specifications, see Section 5.8.2.
An external source must supply the slow clock and connect to the SLOW_CLK_IN pin (for example, the host or external crystal oscillator). The source must be a digital signal in the range of 0 V to 1.8 V. The accuracy of the slow-clock frequency must be 32.768 kHz ±250 ppm for Bluetooth use (as specified in the Bluetooth specification). The external slow clock must be stable within 64 slow-clock cycles (2 ms) following the release of nSHUTD.
An external clock source is fed to an internal pulse-shaping cell to provide the fast-clock signal for the device. The device incorporates an internal, automatic clock-scheme detection mechanism that automatically detects the fast-clock scheme used and configures the FREF cell accordingly. This mechanism ensures that the electrical characteristics (loading) of the fast-clock input remain static regardless of the scheme used and eliminates any power-consumption penalty-versus-scheme used.
The frequency variation of the fast-clock source must not exceed ±20 ppm (as defined by the Bluetooth specification).
The external clock can be AC- or DC-coupled, sine or square wave.
Figure 6-2 and Figure 6-3 show the clock configuration when using a square wave, DC-coupled external source for the fast-clock input.
NOTE
A shunt capacitor with a range of 10 nF must be added on the oscillator output to reject high harmonics and shape the signal to be close to a sinusoidal waveform.
TI recommends using only a dedicated LDO to feed the oscillator. Do not use the same VIO for the oscillator and the CC2564C device.
Figure 6-2 Clock Configuration (Square Wave, DC-Coupled)
Figure 6-3 External Fast Clock (Square Wave, DC-Coupled)
Figure 6-4 and Figure 6-5 show the clock configuration when using a sine wave, DC-coupled external source for the fast clock input.
Figure 6-4 Clock Configuration (Sine Wave, DC-Coupled)
Figure 6-5 External Fast Clock (Sine Wave, DC-Coupled)
Figure 6-6 and Figure 6-7 show the configuration when using a sine wave, AC-coupled external source for the fast-clock input.
Figure 6-6 Clock Configuration (Sine Wave, AC-Coupled)
Figure 6-7 External Fast Clock (Sine Wave, AC-Coupled)
In cases where the input amplitude is greater than 1.6 Vp-p, the amplitude can be reduced to within limits. Using a small series capacitor forms a voltage divider with the internal input capacitance of approximately 2 pF to provide the required amplitude at the device input.
The CC2564C device incorporates an internal crystal oscillator buffer to support a crystal-based fast-clock scheme. The supported crystal frequencies are 26 and 38.4 MHz.
The frequency accuracy of the fast-clock source must not exceed ±20 ppm (including the accuracy of the capacitors, as specified in the Bluetooth specification).
Figure 6-8 shows the recommended fast-clock circuitry.
Figure 6-8 Fast-Clock Crystal Circuit
Table 6-1 lists component values for the fast-clock crystal circuit.
The CC2564C device is the third generation of Bluetooth single-chip devices using DRP architecture from TI. Modifications and new features added to the DRP further improve radio performance.
Figure 6-9 shows the DRP block diagram.
Figure 6-9 DRP Block Diagram
The receiver uses near-zero-IF architecture to convert the RF signal to baseband data. The signal received from the external antenna is input to a single-ended low-noise amplifier (LNA) and passed to a mixer that downconverts the signal to IF, followed by a filter and amplifier. The signal is then quantized by a sigma-delta analog-to-digital converter (ADC) and further processed to reduce the interference level.
The demodulator digitally downconverts the signal to zero-IF and recovers the data stream using an adaptive-decision mechanism. The demodulator includes EDR processing with:
New features include:
The transmitter is an all-digital, sigma-delta phase-locked loop (ADPLL) based with a digitally controlled oscillator (DCO) at 2.4 GHz as the RF clock. The transmitter directly modulates the digital PLL. The power amplifier is also digitally controlled. The transmitter uses the polar-modulation technique. While the phase-modulated control word is fed to the ADPLL, the amplitude-modulated controlled word is fed to the class-E amplifier to generate a Bluetooth standard-compliant RF signal.
New features include:
The CC2564C device incorporates one UART module dedicated to the HCI transport layer. The HCI transports commands, events, and ACL between the device and the host using HCI data packets.
The CC2564C device supports the H4 protocol (4-wire UART) with hardware flow control and the H5 protocol (3-wire UART) with software flow control. The CC2564C device automatically detects the protocol on reception of the first command.
The maximum baud rate of the UART module is 4 Mbps; however, the default baud rate after power up is set to 115.2 kbps. The baud rate can thereafter be changed with a VS command. The device responds with a command complete event (still at 115.2 kbps), after which the baud rate change occurs.
The UART module includes the following features:
Table 6-2 lists the UART module default settings.
| PARAMETER | VALUE |
|---|---|
| Bit rate | 115.2 kbps |
| Data length | 8 bits |
| Stop bit | 1 |
| Parity | None |
The H4 UART Interface includes four signals:
Flow control between the host and the CC2564C device is bytewise by hardware.
Figure 6-10 shows the H4 UART interface.
Figure 6-10 H4 UART Interface
When the UART RX buffer of the device passes the flow control threshold, it sets the HCI_RTS signal high to stop transmission from the host.
When the HCI_CTS signal is set high, the device stops transmission on the interface. If HCI_CTS is set high while transmitting a byte, the device finishes transmitting the byte and stops the transmission.
The H4 protocol device includes a mechanism that handles the transition between active mode and sleep mode. The protocol occurs through the CTS and RTS UART lines and is known as the enhanced HCI low level (eHCILL) power-management protocol.
For more information on the H4 UART protocol, see Volume 4 Host Controller Interface, Part A UART Transport Layer of the Bluetooth Core Specifications
(www.bluetooth.org/en-us/specification/adoptedspecifications).
The H5 UART interface consists of three signals (see Figure 6-11):
Figure 6-11 H5 UART Interface
The H5 protocol supports the following features:
For more information on the H5 UART protocol, see Volume 4 Host Controller Interface, Part D Three- Wire UART Transport Layer of the Bluetooth Core Specifications
(www.bluetooth.org/en-us/specification/adoptedspecifications).
The codec interface is a fully programmable port to support seamless interfacing with different PCM and I2S codec devices. The interface includes the following features:
The interface includes four signals:
The CC2564C device can be the master of the interface when generating the Clock and Frame_Sync signals or the slave when receiving these two signals.
For slave mode, clock input frequencies of up to 15 MHz are supported. At clock rates above 12 MHz, the maximum data burst size is 32 bits.
For master mode, the device can generate any clock frequency from 64 kHz to 4.096 MHz.
When the codec interface is configured to support the I2S protocol, these settings are recommended:
The data format is fully configurable:
The codec interface handles frame-idle periods, during which the clock pauses and becomes 0 at the end of the frame after all data are transferred.
The device supports frame-idle periods both as master and slave of the codec bus.
When the device is the master of the interface, the frame-idle period is configurable. There are two configurable parameters:
The delta between Clk_Idle_Start and Clk_Idle_End is the clock idle period.
For example, for clock rate = 1 MHz, frame sync period = 10 kHz, Clk_Idle_Start = 60, Clk_Idle_End = 90.
Between both Frame_Sync signals there are 70 clock cycles (instead of 100). The clock idle period starts 60 clock cycles after the beginning of the frame and lasts 90 – 60 = 30 clock cycles. Thus, the idle period ends 100 – 90 = 10 clock cycles before the end of the frame. The data transmission must end before the beginning of the idle period.
Figure 6-12 shows the frame idle timing.
Figure 6-12 Frame Idle Period
The codec interface of the device can work on the rising or the falling edge of the clock and can sample the Frame_Sync signal and the data at inversed polarity.
Figure 6-13 shows the operation of a falling-edge-clock type of codec. The codec is the master of the bus. The Frame_Sync signal is updated (by the codec) on the falling edge of the clock and is therefore sampled (by the device) on the next rising clock. The data from the codec is sampled (by the device) on the falling edge of the clock.
Figure 6-13 Negative Clock Edge Operation
Figure 6-14 shows a 2-channel bus in which the two channels have different word sizes and arbitrary positions in the bus frame.
NOTE:
FT stands for frame timer.The CC2564C device contains an embedded coprocessor that can be used for multiple purposes (see Figure 1-1). The CC2564C device uses the coprocessor to perform the LE functionality or to execute the assisted HFP 1.6 (WBS) or assisted A2DP functions. Only one of these functions can be executed at a time because they all use the same resources (that is, the coprocessor; see Table 3-1 for the modes of operation supported by each device).
This section describes the assisted HFP 1.6 (WBS) and assisted A2DP modes of operation. These modes of operation minimize host processing and power by taking advantage of the device coprocessor to perform the voice and audio SBC processing required in HFP 1.6 (WBS) and A2DP profiles. This section also compares the architecture of the assisted modes with the common implementation of the HFP 1.6 and A2DP profiles.
The assisted HFP 1.6 (WBS) and assisted A2DP modes of operation comply fully with the HFP 1.6 and A2DP Bluetooth specifications. For more information on these profiles, see the corresponding Bluetooth Profile Specification (www.bluetooth.org/en-us/specification/adopted-specifications).
The HFP 1.6 Profile Specification adds the requirement for WBS support. The WBS feature allows twice the voice quality versus legacy voice coding schemes at the same air bandwidth (64 kbps). This feature is achieved using a voice sampling rate of 16 kHz, a modified subband coding (mSBC) scheme, and a packet loss concealment (PLC) algorithm. The mSBC scheme is a modified version of the mandatory audio coding scheme used in the A2DP profile with the parameters listed in Table 6-3.
| PARAMETER | VALUE |
|---|---|
| Channel mode | Mono |
| Sampling rate | 16 kHz |
| Allocation method | Loudness |
| Subbands | 8 |
| Block length | 15 |
| Bitpool | 26 |
The assisted HFP 1.6 mode of operation implements this WBS feature on the embedded CC2564C coprocessor. That is, the mSBC voice coding scheme and the PLC algorithm are executed in the CC2564C coprocessor rather than in the host, thus minimizing host processing and power. One WBS connection at a time is supported, and WBS and NBS connections cannot be used simultaneously in this mode of operation. Figure 6-15 shows the architecture comparison between the common implementation of the HFP 1.6 profile and the assisted HFP 1.6 solution.
Figure 6-15 HFP 1.6 Architecture Versus Assisted HFP 1.6 Architecture
For detailed information on the HFP 1.6 profile, see the Hands-Free Profile 1.6 Specification (www.bluetooth.org/en-us/specification/adopted-specifications).
The advanced audio distribution profile (A2DP) enables wireless transmission of high-quality mono or stereo audio between two devices. A2DP defines two roles:
A typical use case streams music from a tablet, phone, or PC (the A2DP source) to headphones or speakers (the A2DP sink). This section describes the architecture of these roles and compares them with the corresponding assisted-A2DP architecture. To use the air bandwidth efficiently, the audio data must be compressed in a proper format. The A2DP mandates support of the SBC scheme. Other audio coding algorithms can be used; however, both Bluetooth devices must support the same coding scheme. SBC is the only coding scheme spread out in all A2DP Bluetooth devices; thus, it is the only coding scheme supported in the assisted A2DP modes. Table 6-4 lists the recommended parameters for the SBC scheme in the assisted A2DP modes.
| SBC ENCODER SETTINGS(1) | MID QUALITY | HIGH QUALITY | ||||||
|---|---|---|---|---|---|---|---|---|
| MONO | JOINT STEREO | MONO | JOINT STEREO | |||||
| Sampling frequency (kHz) | 44.1 | 48 | 44.1 | 48 | 44.1 | 48 | 44.1 | 48 |
| Bitpool value | 19 | 18 | 35 | 33 | 31 | 29 | 53 | 51 |
| Resulting frame length (bytes) | 46 | 44 | 83 | 79 | 70 | 66 | 119 | 115 |
| Resulting bit rate (Kbps) | 127 | 132 | 229 | 237 | 193 | 198 | 328 | 345 |
The SBC scheme supports a wide variety of configurations to adjust the audio quality. Table 6-5 through Table 6-12 list the supported SBC capabilities in the assisted A2DP modes.
| CHANNEL MODE | STATUS |
|---|---|
| Mono | Supported |
| Dual channel | Supported |
| Stereo | Supported |
| Joint stereo | Supported |
| SAMPLING FREQUENCY (kHz) | STATUS |
|---|---|
| 16 | Supported |
| 44.1 | Supported |
| 48 | Supported |
| BLOCK LENGTH | STATUS |
|---|---|
| 4 | Supported |
| 8 | Supported |
| 12 | Supported |
| 16 | Supported |
| SUBBANDS | STATUS |
|---|---|
| 4 | Supported |
| 8 | Supported |
| ALLOCATION METHOD | STATUS |
|---|---|
| SNR | Supported |
| Loudness | Supported |
| BITPOOL RANGE | STATUS |
|---|---|
| Assisted A2DP sink: 2–54 | Supported |
| Assisted A2DP source: 2–57 | Supported |
| L2CAP MTU SIZE (BYTES) | STATUS |
|---|---|
| Assisted A2DP sink: 260–800 | Supported |
| Assisted A2DP source: 260–1021 | Supported |
| ITEM | VALUE | STATUS |
|---|---|---|
| A2DP content protection | Protected | Not supported |
| AVDTP service | Basic type | Supported |
| L2CAP mode | Basic mode | Supported |
| L2CAP flush | Nonflushable | Supported |
For detailed information on the A2DP profile, see the A2DP Profile Specification at Adopted Bluetooth Core Specifications.
The role of the A2DP sink is to receive the audio stream in an A2DP Bluetooth connection. In this role, the A2DP layer and its underlying layers are responsible for link management and data decoding. To handle these tasks, two logic transports are defined:
The assisted A2DP takes advantage of this modularity to handle the data packet logic transport in the CC2564C device. First, the assisted A2DP implements a light L2CAP layer (L-L2CAP) and light AVDTP layer (L-AVDTP) to defragment the packets. Then the assisted A2DP performs the SBC decoding on-chip to deliver raw audio data through the device PCM–I2S interface. Figure 6-16 shows the comparison between a common A2DP sink architecture and the assisted A2DP sink architecture.
Figure 6-16 A2DP Sink Architecture Versus Assisted A2DP Sink Architecture
For more information on the A2DP sink role, see the A2DP Profile Specification at Adopted Bluetooth Core Specifications.
The role of the A2DP source is to transmit the audio stream in an A2DP Bluetooth connection. In this role, the A2DP layer and its underlying layers are responsible for link management and data encoding. To handle these tasks, two logic transports are defined:
The assisted A2DP takes advantage of this modularity to handle the data packet logic transport in the CC2564C device. First, the assisted A2DP encodes the raw data from the CC2564C PCM–I2S interface using an on-chip SBC encoder. Then the assisted A2DP implements an L-L2CAP layer and an L-AVDTP layer to fragment and packetize the encoded audio data. Figure 6-17 shows the comparison between a common A2DP source architecture and the assisted A2DP source architecture.
Figure 6-17 A2DP Source Architecture Versus Assisted A2DP Source Architecture
For more information on the A2DP source role, see the A2DP Profile Specification at Adopted Bluetooth Core Specifications.
The CC2564C device complies with the Bluetooth 4.2 specification up to the HCI layer (for family members and technology supported, see Table 3-1):
The CC2564C device complies with the Bluetooth 4.2 specification up to the HCI layer (for the family members and technology supported, see Table 3-1):
NOTE
The assisted modes (HFP 1.6 and A2DP) are not available when Bluetooth low energy is enabled.
Figure 6-18 shows the Bluetooth transport layers.
Figure 6-18 Bluetooth Transport Layers
The CC2564C device includes the following changes: