ZHCSHU6L march 2018 – august 2023 BQ77915
PRODUCTION DATA
The BQ77915 device supports the ability to greatly reduce production test time by cutting down on protection fault delay times. To shorten fault times, place the BQ77915 device into Customer Test Mode (CTM). CTM is triggered by raising VDD to VCTM voltage above the highest cell input pin (that is, VC5) for tCTM_ENTRY time.
The CTM is expected to be used in single-chip designs only. CTM is not supported for stacked designs. Once the device is in CTM, all fault delays and non-current fault's recovery delay times reduce to a value of tCTM_DELAY. The fault recovery time for overcurrent faults (OCD1, OCD2, OCC, and SCD) is reduced to tCTM_OC_REC.
Verification of protection fault functionality can be accomplished in a reduced timeframe in CTM. Reducing the VDD voltage to the same voltage applied to the highest-cell input pin for tCTM_ENTRY will exit CTM.
In CTM, with reduced time for all internal delays, qualification of all faults will be reduced to a single instance. Thus, in this mode, fault-condition qualification is more susceptible to transients, so take care to have fault conditions clearly and cleanly applied during test mode to avoid false triggering of fault conditions during CTM.