ZHCSMK4A september 2022 – july 2023 ADS131B26-Q1
PRODUCTION DATA
Gain drift is defined as the change of gain error over the specified temperature range. Gain drift is calculated using the box method in which a box is formed over the maximum and minimum gain errors and over the specified temperature range. The box method specifies limits for the temperature error but does not specify the exact shape and slope of the device under test. For that reason, gain drift is specified as a positive number only, even though the drift can possibly be negative. Equation 2 describes the gain drift calculation using the box method.
where: