ZHCSEE8B December 2015 – April 2017 ADC14X250
PRODUCTION DATA.
The ADC14X250 device is a single channel analog-to-digital converter (ADC) composed of pipelined stages and followed by a back-end JESD204B interface. The ADC core is preceded by an input buffer and imbalance correction circuit at the analog input and is provided with the necessary reference voltages with internal drivers that require no external components. The analog input common-mode is also internally regulated.
A DC offset correction block is disabled by default, but may also be enabled at the ADC core output to remove DC offset. Processed data is passed into the JESD204B interface where the data is framed, encoded, serialized, and output on one lane per channel. Data is serially transmitted by configurable high-speed voltage mode drivers.
The sampling clock is derived from the CLKIN input via a low-noise receiver and clock divider. The CLKIN, SYSREF, and SYNCb inputs provide the device clock, sysref, and sync~ signals to the JESD204B interface, which are used to derive the internal local frame and local multi-frame clocks and establish the serial link.
Features of the ADC14X250 device are configurable through the 4-wire SPI.
The ADC performance can be sensitive to amplitude and phase imbalance of the input differential signal and therefore integrates a front-end balance correction circuit to optimize the second-order distortion (HD2) performance of the ADC in the presence of an imbalanced input signal. 4-bit control of the phase mismatch and 3-bit control of the amplitude mismatch corrects the input mismatch before the input buffer. A simplified diagram of the amplitude and phase correction circuit at the ADC input is shown in Figure 32.
Figure 32. Simplified Input Differential Balance Correction Circuit
Amplitude correction is achieved by varying the single-ended termination resistance of each input while maintaining constant total differential resistance, thereby adjusting the amplitude at each input but leaving the differential swing constant. Phase correction, also considered capacitive balance correction, varies the capacitive load at the ADC input, thereby correcting a phase imbalance by creating a bandwidth difference between the analog inputs that minimally affects amplitude. This function is useful for correcting the balance of transformers or filters that drive the ADC analog inputs. Figure 33 shows the measured HD2 resulting from an example 240-MHz imbalanced signal input into the ADC14X250 device recorded over the available amplitude and phase correction settings, demonstrating the optimization of HD2. Performance parameters in the Electrical Characteristics: Dynamic Converter Performance are characterized with the amplitude and phase correction settings in the default condition.
Figure 33. Gain and Phase Imbalance HD2 Optimization
An input clock divider allows a high frequency clock signal to be distributed throughout the system and locally divided down at the ADC device so that coupling of signals at common intermediate frequencies into other parts of the system can be avoided. The frequency at the CLKIN input may be divided down to the sampling rate of the ADC by factors of 1, 2, 4, or 8. Changing the clock divider setting initiates a JESD204 link re-initialization and requires re-calibration of the ADC if the sampling rate is changed from the rate during the previous calibration.
When the signal at the SYSREF input is not actively toggling periodically, the SYSREF signal is considered to be in an idle state. The idle state is recommended at any time the ADC14X250 spurious performance must be maximized. When the SYSREF signal is in the idle state for longer than 1 µs, an undesirable offset voltage may build up across the AC coupling capacitors between the SYSREF transmitter and the ADC14X250 device input. This offset voltage creates a signal threshold problem, requires a long time to dissipate, and therefore prevents quick transition of the SYSREF signal out of the idle state. Two features are provided as a solution and are shown in Figure 50, namely the SYSREF offset feature and SYSREF detection gate.
In the case that the SYSREF signal idle state has a 0-V differential value, or if the ADC14X250 device must be insensitive to noise that may appear on the SYSREF signal, then the SYSREF detection gate may be used. The detection gate is the AND gate shown in Figure 50 that enables or disables propagation of the SYSREF signal through to the internal device logic. If the detection gate is disabled and a false edge appears at the SYSREF input, the signal does not disrupt the internal clock alignment. Note that the SYSREF detection gate is disabled by default; therefore, the device does not respond to a SYSREF edge until the detection gate is enabled.
The SYSREF offset and detection gate features are both controlled through the SPI.
DC offset correction is provided using a digital high-pass IIR filter at the immediate output of the ADC core. The DC offset correction is bypassed by default, but may be enabled and configured via the SPI. The 3-dB bandwidth of the IIR digital correction filter may be set to four different low-frequency values. When DC offset correction is enabled, any signal in the stop-band of the high-pass filter is attenuated. The settling time of the DC offset correction is approximately equal to the inverse of the 3-dB bandwidth setting.
The differential drivers of the ADC14X250 device that output the serial JESD204B data are voltage mode drivers with amplitude control and de-emphasis features that may be configured through the SPI for a variety of different channel applications. Eight amplitude control (VOD) and eight de-emphasis control (DEM) settings are available. Both VOD and DEM register fields must be configured to optimize the noise performance of the serial interface for a particular lossy channel.
The output common-mode of the driver varies with the configuration of the output swing. Therefore, AC coupling is strongly recommended between the ADC14X250 device and the device receiving the serial data.
De-emphasis of the differential output is provided as a form of continuous-time linear equalization that imposes a high-pass frequency response onto the output signal to compensate for frequency-dependent attenuation as the signal propagates through the channel to the receiver. In the time-domain, the de-emphasis appears as the bit transition transient followed by an immediate reduction in the differential amplitude, as shown in Figure 34. The characteristic appearance of the waveform changes with differential amplitude and the magnitude of de-emphasis applied. The serial lane rate determines the available period of time during which the de-emphasis transient settles. However, the lane rate does not affect the settling behavior of the applied de-emphasis.
Figure 34. De-emphasis of the Differential Output Signal
Table 1 indicates the typical measured values for the de-emphasis range, where the de-emphasis value is measured as the ratio (in units of [dB]) between the peak voltage after the signal transition to the settled voltage value in one bit period. The data rate for this measurement is 1.2 Gb/s to allow settling of the de-emphasis transient. Table 1 illustrates the actual de-emphasis value in terms of voltage attenuation and shows dependence on the amplitude setting, but does not reflect the optimal amplitude setting (VOD) and de-emphasis setting (DEM) for a particular lossy channel. Table 2 shows the amplitude of the differential signal swing during its settled state after the transition transient. The measurement is performed at 1.2 Gb/s and the units are in differential peak-to-peak mV.
| DEM | |||||||||
|---|---|---|---|---|---|---|---|---|---|
| 0 | 1 | 2 | 3 | 4 | 5 | 6 | 7 | ||
| VOD | 0 | 0 | –0.2 | –1.1 | –2.2 | –3.0 | –4.3 | –5.6 | –8.5 |
| 1 | 0 | –0.4 | –1.7 | –2.9 | –3.8 | –5.1 | –6.5 | –9.6 | |
| 2 | 0 | –0.7 | –2.2 | –3.5 | –4.5 | –5.9 | –7.4 | –10.4 | |
| 3 | 0 | –1.0 | –2.8 | –4.2 | –5.2 | –6.7 | –8.1 | –11.2 | |
| 4 | 0 | –1.4 | –3.4 | –4.9 | –5.9 | –7.4 | –8.9 | –12.1 | |
| 5 | 0 | –1.7 | –3.9 | –5.5 | –6.5 | –8.0 | –9.5 | –12.7 | |
| 6 | 0 | –2.1 | –4.4 | –6.0 | –7.1 | –8.6 | –10.2 | –13.4 | |
| 7 | 0 | –2.5 | –4.9 | –6.5 | –7.6 | –9.2 | –10.7 | –14.0 | |
| DEM | |||||||||
|---|---|---|---|---|---|---|---|---|---|
| 0 | 1 | 2 | 3 | 4 | 5 | 6 | 7 | ||
| VOD | 0 | 570 | 550 | 500 | 440 | 400 | 350 | 300 | 210 |
| 1 | 660 | 630 | 550 | 470 | 430 | 370 | 310 | 220 | |
| 2 | 750 | 690 | 580 | 500 | 450 | 380 | 320 | 230 | |
| 3 | 840 | 750 | 610 | 520 | 460 | 390 | 330 | 230 | |
| 4 | 940 | 800 | 630 | 530 | 470 | 400 | 340 | 230 | |
| 5 | 1020 | 840 | 650 | 550 | 480 | 410 | 340 | 240 | |
| 6 | 1110 | 870 | 670 | 560 | 490 | 410 | 340 | 240 | |
| 7 | 1200 | 900 | 680 | 570 | 500 | 420 | 350 | 240 | |
After power-up, the ADC14X250 device detects that the supplies and clock are valid, waits for a power-up delay, and then performs a calibration of the ADC core automatically. The power-up delay is 8.4 × 106 sampling clock cycles or 33.6 ms at a 250-MSPS sampling rate. The calibration requires approximately 1.0 × 106 sampling clock cycles.
If the system requires that the ADC14X250 input clock divider value (CLKDIV) is set to 2, 4, or 8, then ADC calibration must be performed manually after CLKDIV has been set to the desired value. Manual calibration is performed by changing to power down mode, returning to normal operation, and monitoring the CAL_DONE bit in the JESD_STATUS register until calibration is complete. As an alternative to monitoring CAL_DONE, the system may wait 1.5 × 106 sampling clock cycles until calibration is complete.
Re-calibration is not required across the supported operating temperature range to maintain functional performance, but it is recommended for large changes in ambient temperature to maintain optimal dynamic performance. Changing the sampling rate always requires re-calibration of the ADC core. For more information about device modes, see Power-Down and Sleep Modes.
Data may be output in the serial stream as 2’s complement format by default or optionally as offset binary. This formatting is configured through the SPI and is performed in the data path prior to JESD204B data framing, scrambling and 8b/10b encoding.
The ADC14X250 device supports a feature set of the JESD204B standard targeted to its intended applications but does not implement all the flexibility of the standard. Table 3 summarizes the level of feature support.
| Feature | Supported | Not Supported |
|---|---|---|
| Subclass |
|
|
| Device Clock (CLKIN) and SYSREF |
|
|
| Latency |
|
|
| Electrical layer features |
|
|
| Transport layer features and configuration |
|
|
| Data link layer features |
|
|
The transport layer features supported by the ADC14X250 device are a subset of possible features described in the JESD204B standard. The configuration options are intentionally simplified to provide the lowest power and most easy-to-use solution.
The ADC14X250 outputs all digital data on a single JESD204B serial lane. The serial-data lane transmits at 20 times the sampling rate. A 250 MSPS sampling rate corresponds to a 5.0 Gb/s per lane rate.
The format of the data arranged in a frame is fixed. The octets per frame (F), samples per frame (S), and high-density mode (HD) parameters are not independently configurable. The N, N’, CS, CF, M, and HD parameters are fixed and not configurable. Figure 35 shows the data format.
Figure 35. Transport Layer Definitions for the Supported-Lane Configurations
Table 4 summarizes the information transmitted during the initial lane alignment (ILA) sequence. Mapping of these parameters into the data stream is described in the JESD204B standard.
| Parameter | Description | Logical Value | Encoded Value | |
|---|---|---|---|---|
| ADJCNT | DAC LMFC adjustment | 0 | 0 | |
| ADJDIR | DAC LMFC adjustment direction | 0 | 0 | |
| BID | Bank ID | 0 | 0 | |
| CF | Number of control words per frame clock period per link | 0 | 0 | |
| CS | Number of control bits per sample | 0 | 0 | |
| DID | Device identification number | 0 | 0 | |
| F | Number of octets per frame (per lane)(1) | 2 | 1 | |
| HD | High-density format | 0 | 0 | |
| JESDV | JESD204 version | 1 | 1 | |
| K | Number of frames per multi-frame(1) | Set by register as 9 to 32 | 8 to 31 | |
| L | Number of lanes per link(1) | 1 | 0 | |
| LID | Lane identification number | 0 | 0 | |
| M | Number of converters per device(1) | 1 | 1 | |
| N | Converter resolution (1) | 16 | 15 | |
| N’ | Total number of bits per sample(1) | 16 | 15 | |
| PHADJ | Phase adjustment request to DAC | 0 | 0 | |
| S | Number of samples per converter per frame cycle(1) | 1 | 0 | |
| SCR | Scrambling enabled | Set by register as 0 (disabled) or 1 | 0 or 1 | |
| SUBCLASSV | Device subclass version | 1 | 1 | |
| RES1 | Reserved field 1 | 0 | 0 | |
| RES2 | Reserved field 2 | 0 | 0 | |
| FCHK | Checksum | 34 + (K-1) + SCR | ||
Scrambling of the output serial data is supported and conforms to the JESD204B standard. Scrambling is disabled by default, but may be enabled via the SPI. When scrambling is enabled, the ADC14X250 device supports the early synchronization option by the receiver during the ILA sequence, although the ILA sequence data is never scrambled.
The SPI may enable the following test pattern sequences. Short- and long-transport layer, RPAT, and JSPAT sequences are not supported.
| Test Pattern | Description | Common Purpose |
|---|---|---|
| D21.5 | Alternating 1 and 0 pattern (101010...) | Jitter or system debug |
| K28.5 | Continuous K28.5 symbols | System debug |
| Repeated ILA | ILA repeats indefinitely | System debug |
| Ramp | After ILA, a sample ramp is transmitted with programmable step. The 16-bit output word fully spans both octets that compose a sample. | System debug and transport layer verification |
| PRBS | PRBS 7/15/23 Complies with ITU-T O.150 specification and is compatible with J-BERT equipment | Jitter and bit error rate testing |
A JESD204B link is established via link initialization, which involves the following steps: frame alignment, code group synchronization, and initial lane synchronization. These steps are shown in Figure 36. Link initialization must occur between the transmitting device (ADC14X250) and receiving device before sampled data may be transmitted over the link. The link initialization steps described here are specifically for the ADC14X250 device, supporting JESD204B subclass 1.
Figure 36. Link-initialization Timing and Flow Diagram
The Frame Alignment step requires alignment of the frame and local multi-frame clocks within the ADC14X250 device to an external reference. This is accomplished by providing the device clock and SYSREF clock to the CLKIN and SYSREF inputs, respectively. The ADC14X250 device aligns its frame clock and LMFC to any SYSREF rising edge event, offset by a SYSREF-to-LMFC propagation delay.
The SYSREF signal must be source synchronous to the device clock; therefore, the SYSREF rising edge must meet setup and hold requirements relative to the signal at the CLKIN input. If these requirements cannot be met, then the alignment of the internal frame and multi-frame clocks cannot be ensured. As a result, a link may still be established, but the latency through the link cannot be deterministic. Frame alignment may occur at any time; although, a re-alignment of the internal frame clock and LMFC will break the link. Note that frame alignment is not required for the ADC14X250 device to establish a link because the device automatically generates the clocks on power-up with unknown phase alignment.
Code Group Synchronization is initiated when the receiver sends a synchronization request by asserting the SYNCb input of the ADC14X250 device to a logic low state (SYNCb+ < SYNCb–). After the SYNCb assertion is detected, the ADC14X250 device outputs K28.5 symbols on all serial lanes that are used by the receiver to synchronize and time align its clock and data recovery (CDR) block to the known symbols. The SYNCb signal must be asserted for at least 4 frame clock cycles otherwise the event is ignored by the ADC14X250 device. Code group synchronization is completed when the receiver de-asserts the SYNCb signal to a logic high state.
After the ADC14X250 detects a de-assertion of its SYNCb input, the Initial Lane Synchronization step begins on the following LMFC boundary. The ADC14X250 device outputs 4 multi-frames of information that compose the ILA sequence. This sequence contains information about the data transmitted on the link. The initial lane synchronization step and link initialization conclude when the ILA is finished and immediately transitions into Data Transmission. During data transmission, valid sampled data is transmitted across the link until the link is broken.
Figure 37. Device Start-Up and JESD204B Link Synchronization Flow Chart
The flowchart in Figure 37 describes how the ADC14X250 device initializes the JESD204B link and reacts to changes in the link. After the ADC core calibration is finished, the ADC14X250 device begins with PLL calibration and link initialization using a default frame clock and LMFC alignment by sending K28.5 characters. PLL calibration requires approximately 153×103 sampling clock cycles. If SYNCb is not asserted, then the device immediately advances to the ILA sequence at the next LMFC boundary. Whereas, if SYNCb is asserted, then the device continues to output K28.5 characters until SYNCb is de-asserted.
When a SYSREF rising edge event is detected, then the ADC14X250 device compares the SYSREF event to the current alignment of the LMFC. If the SYSREF event is aligned to the current LMFC alignment, then no action is taken and the device continues to output data. If misalignment is detected, then the SYSREF event is compared to the frame clock. If misalignment of the frame clock is also detected, then the clocks are re-aligned and the link is re-initialized. If the frame clock is not misaligned, then the frame clock alignment is not updated. In the cases that a SYSREF event causes a link re-initialization, the ADC14X250 device begins sending K28.5 characters without a SYNCb assertion and immediately transitions to the ILA sequence on the next LMFC boundary unless the SYNCb signal is asserted. Anytime the frame clock and LMFC are re-aligned, the serializer PLL must calibrate before code group synchronization begins. SYSREF events must not occur during ADC14X250 device power-up, ADC calibration, or PLL calibration. The JESD_STATUS register is available to check the status of the ADC14X250 device and the JESD204B link.
If a SYNCb assertion is detected for at least 4 frame clock cycles, the ADC14X250 device immediately breaks the link and sends K28.5 characters until the SYNCb signal is de-asserted.
When exiting sleep mode, the frame clock and LMFC are started with a default (unknown) phase alignment, PLL calibration is performed, and the device immediately transitions into sending K28.5 characters.
The JESD204B sync~ signal can be directed to the internal JESD204B core block via two different input paths: via the external pins or SPI. The selection MUX is controlled using the SYNC_SEL register field and sync~ control is performed using the JSYNC_N register field via SPI . By default, the signal is routed from the external SYNCb+/- pins and writes to the JSYNC_N register field are ignored.
Optionally, the signal may be routed via SPI by setting the register field SYNC_SEL = 1. In this mode, signals at the external SYNCb+/- pins are ignored and the sync~ signal is written to the JSYNC_N register field.
The SPI allows access to the internal configuration registers of the ADC through read and write commands to a specific address. The interface protocol has a 1-bit command, 15-bit address word and 8-bit data word as shown in Figure 38. A read or write command is 24 bits in total, starting with the read or write command bit where 0 indicates a write command and 1 indicates a read command. The read or write command bit is clocked into the device on the first rising edge of SCLK after CSb is asserted to 0. During a write command, the 15-bit address and 8-bit data values follow the read or write bit MSB-first and are latched on the rising edge of SCLK. During a read command, the SDO output is enabled shortly after the 16th rising edge of SCLK and outputs the read value MSB first before the SDO output is returned to a high impedance state. The read or write command is completed on the SCLK rising edge on which the data word’s LSB is latched. CSb may be de-asserted to 1 after the LSB is latched into the device.
The SPI allows command streaming where multiple commands are made without de-asserting CSb in-between commands. The commands in the stream must be of similar types, either read or write. Each subsequent command applies to the register address adjacent to the register accessed in the previous command. The address order can be configured as either ascending or descending. Command streaming is accomplished by immediately following a completed command with another set of 8 rising edges of SCLK without de-asserting CSb. During a write command, an 8-bit data word is input on the SDI input for each subsequent set of SCLK edges. During a read command, data is output from SDO for each subsequent set of SCLK edges. Each subsequent command is considered finished after the 8th rising edge of SCLK. De-asserting CSb aborts an incomplete command.
The SDO output is high impedance at all times other than during the final portion of a read command. During the time that the SDO output is active, the logic level is determined by a configuration register. The SPI output logic level must be properly configured after power up and before making a read command to prevent damaging the receiving device or any other device connected to the SPI bus. Until the SPI_CFG register is properly configured, voltages on the SDO output may be as high as the VA3.0 supply during a read command. The default state of SDO is to output 3 V logic levels during a read command. The SDI, SCLK, and CSB pins are all 1.2-V to 3-V logic compatible.
Figure 38. Serial Interface Protocol
Power-down and sleep modes are provided to allow the user to reduce the power consumption of the device without disabling power supplies. Both modes reduce power consumption by the same amount but they differ in the amount of time required to return to normal operation. Upon changing from Power Down back to Normal operation, an ADC calibration routine is performed. Waking from sleep mode does not perform ADC calibration (see ADC Core Calibration for more details). Neither power-down mode nor sleep mode resets configuration registers.
| Register | ADDRESS | DFLT | b[7] | b[6] | b[5] | b[4] | b[3] | b[2] | b[1] | b[0] | |
|---|---|---|---|---|---|---|---|---|---|---|---|
| CONFIG_A | 0x0000 | 0x3C | SR | Res (0) | ASCEND | Res (1) | PAL[3:0] | ||||
| Address 0x0001 Reserved | |||||||||||
| DEVICE _CONFIG | 0x0002 | 0x00 | Reserved (000000) | PD_MODE[1:0] | |||||||
| CHIP_TYPE | 0x0003 | 0x03 | Reserved (0000) | CHIP_TYPE[3:0] | |||||||
| CHIP_ID | 0x0004 | 0x01 | CHIP_ID[7:0] | ||||||||
| 0x0005 | 0x00 | CHIP_ID[15:8] | |||||||||
| CHIP _VER | 0x0006 | 0x00 | CHIP_VER[7:0] | ||||||||
| Address 0x0007-0x000B Reserved | |||||||||||
| VENDOR_ID | 0x000C | 0x51 | VENDOR_ID[7:0] | ||||||||
| 0x000D | 0x04 | VENDOR_ID[15:8] | |||||||||
| SPI_CFG | 0x0010 | 0x01 | Reserved (000000) | VSPI[1:0] | |||||||
| OM1 | 0x0012 | 0x81 | DF | Res (00) | IDLE[1:0] | SYS_EN | Res(01) | ||||
| OM2 | 0x0013 | 0x20 | Reserved (001) | CLKDIV | Res (0) | Res (0) | Res (0) | ||||
| IMB_ADJ | 0x0014 | 0x00 | Res (0) | AMPADJ[2:0] | PHADJ[3:0] | ||||||
| Address 0x0015-0x003C Reserved | |||||||||||
| DC_MODE | 0x003D | 0x00 | Reserved (00000) | DC_TC | DC_EN | ||||||
| Address 0x003E-0x0046 Reserved | |||||||||||
| SER_CFG | 0x0047 | 0x00 | Res(0) | VOD[2:0] | Res (0) | DEM[2:0] | |||||
| Address 0x0048-0x005F Reserved | |||||||||||
| JESD_CTRL1 | 0x0060 | 0x7D | SCR _EN | K_M1[4:0] | Res (0) | JESD _EN | |||||
| JESD_CTRL2 | 0x0061 | 0x00 | SYNC_SEL | JSYNC_N | Reserved (00) | JESD_TEST_MODE[3:0] | |||||
| JESD_RSTEP | 0x0062 | 0x01 | JESD_RSTEP[7:0] | ||||||||
| 0x0063 | 0x00 | JESD_RSTEP[15:8] | |||||||||
| Address 0x0064-0x006B Reserved | |||||||||||
| JESD_STATUS | 0x006C | N/A | Res (0) | LINK | SYNC | REALIGN | ALIGN | PLL _LOCK | CAL _DONE | CLK _RDY | |
| Address 0x006D- Reserved | |||||||||||
| Bit | Field | Type | Reset | Description | |
|---|---|---|---|---|---|
| 7 | SR | Read or write | 0 | Setting this soft reset bit causes all registers to be reset to their default state. This bit is self-clearing. | |
| 6 | Reserved | Read or write | 0 | Reserved and must be written with 0. | |
| 5 | ASCEND | Read or write | 1 | Order of address change during streaming reads or writes. 0 : Address is decremented during streaming reads or writes. 1 : Address is incremented during streaming reads or writes (default). |
|
| 4 | Reserved | Read | 1 | Reserved and must be written with 1. | |
| 3:0 | PAL[3:0] | Read or write | 1100 | Palindrome Bits are bit 3 = bit 4, bit 2 = bit 5, bit 1 = bit 6, and bit 0 = bit 7. | |
| Bit | Field | Type | Reset | Description | |
|---|---|---|---|---|---|
| [7:2] | Reserved | Read or write | 000000 | Reserved and must be written with 000000. | |
| [1:0] | PD_MODE [1:0] | Read or write | 00 | Power-down mode 00 : Normal operation (default) 01 : Reserved 10 : Sleep operation (faster resume) 11 : Power-down (slower resume) |
|
| Bit | Field | Type | Reset | Description | |
|---|---|---|---|---|---|
| [7:4] | Reserved | Read or write | 0000 | Reserved and must be written with 0000. | |
| [3:0] | CHIP_TYPE | Read | 0011 | Chip type that always returns 0x3, indicating that the part is a high-speed ADC | |
| Bit | Field | Type | Reset | Description | |
|---|---|---|---|---|---|
| 0x0004[7:0] | CHIP_ID[7:0] | Read | 0x01 | Chip ID least significant word | |
| 0x0005[7:0] | CHIP_ID[15:8] | Read | 0x00 | Chip ID most significant word | |
| Bit | Field | Type | Reset | Description | |
|---|---|---|---|---|---|
| [7:0] | CHIP_VER | Read | 0x00 | Chip version | |
| Bit | Field | Type | Reset | Description | |
|---|---|---|---|---|---|
| 0x000C[7:0] | VENDOR_ID [7:0] |
Read | 0x51 | Vendor ID. Texas Instruments vendor ID is 0x0451. | |
| 0x000D[7:0] | VENDOR_ID [15:8] |
Read | 0x04 | ||
| Bit | Field | Type | Reset | Description | |
|---|---|---|---|---|---|
| [7] | DF | Read or write | 1 | Output data format 0 : Offset binary 1 : Signed 2s complement (default) |
|
| [6:5] | Reserved | Read or write | 00 | Reserved and must be written with 00. | |
| [4:3] | IDLE[1:0] | Read or write | 00 | SYSREF idle state offset configuration. 00 : No offset applied (default) 01 : SYSREF idles low (de-asserted) with –400-mV offset 10 : SYSREF idles high (asserted) with +400-mV offset 11 : Reserved |
|
| [2] | SYS_EN | Read or write | 0 | SYSREF detection gate enable 0 : SYSREF gate is disabled; (input is ignored, default) 1 : SYSREF gate is enabled |
|
| [1:0] | Reserved[1:0] | Read or write | 01 | Reserved. Must be written with 01. | |
| Bit | Field | Type | Reset | Description | |
|---|---|---|---|---|---|
| [7:5] | Reserved | Read or write | 001 | Reserved and must be written with 001. | |
| [4:3] | CLKDIV[1:0] | Read or write | 00 | Clock divider ratio. Sets the value of the clock divide factor, CLKDIV 00 : Divide by 1, CLKDIV = 1 (default) 01 : Divide by 2, CLKDIV = 2 10 : Divide by 4, CLKDIV = 4 11 : Divide by 8, CLKDIV = 8 |
|
| [2:0] | Reserved | Read or write | 000 | Reserved. Must be written with 000. | |
| Bit | Field | Type | Reset | Description | |
|---|---|---|---|---|---|
| [7] | Reserved | Read or write | 0 | Reserved. Must be written with 0. | |
| [6:4] | AMPADJ[2:0] | Read or write | 000 | Analog input amplitude imbalance correction 7 = +30 Ω VIN+, –30 Ω VIN– 6 = +20 Ω VIN+, –20 Ω VIN– 5 = +10 Ω VIN+, –10 Ω VIN– 4 = Reserved 3 = –30 Ω VIN+, +30 Ω VIN– 2 = –20 Ω VIN+, +20 Ω VIN– 1 = –10 Ω VIN+, +10 Ω VIN– 0 = +0 Ω VIN+, –0 Ω VIN– (default) Resistance changes indicate variation of the internal single-ended termination. |
|
| [3:0] | PHADJ[3:0] | Read or write | 0000 | Analog input phase imbalance correction 15 = +1.68 pF VIN– ... 9 = +0.48 pF VIN– 8 = +0.24 pF VIN– 7 = +1.68 pF VIN+ ... 2 = +0.48 pF VIN+ 1 = +0.24 pF VIN+ 0 = +0 pF VIN+, +0 pF VIN– (default) Capacitance changes indicate the addition of internal capacitive load on the given pin. |
|
| DC_MODE (DC Offset Correction Mode) | |||||||
|---|---|---|---|---|---|---|---|
| Bit | Field | Type | Reset | Description | |||
| [7:3] | Reserved | Read or write | 00000 | Reserved and must be written as 00000. | |||
| [2:1] | TC_DC | Read or write | 00 | DC offset filter time constant. The time constant determines the filter bandwidth of the DC high-pass filter. |
|||
| TC_DC | Time Constant (FS = 250 MSPS) | 3-dB Bandwidth (FS = 250 MSPS) | 3-dB Bandwidth (Normalized) | ||||
| 00 | 17 µs | 9.3 kHz | 37e–6 × Fs | ||||
| 01 | 130 µs | 1.2 kHz | 4.9e–6 × Fs | ||||
| 10 | 1.1 ms | 150 Hz | 605e–9 × Fs | ||||
| 11 | 8.4 ms | 19 Hz | 76e–9 × Fs | ||||
| [0] | DC_EN | Read or Write | 0 | DC offset correction enable 0 : Disable DC offset correction 1 : Enable DC offset correction |
|||
| Bit | Field | Type | Reset | Description | ||
|---|---|---|---|---|---|---|
| [7] | Reserved | Read or write | 0 | Reserved. Must be written as 0. | ||
| [6:4] | VOD[2:0] | Read or write | 000 | Serial-lane transmitter driver output differential peak-peak-voltage amplitude. 000 : 0.570 V (default) 001 : 0.660 V 010 : 0.750 V 011 : 0.840 V 100 : 0.940 V 101 : 1.02 V 110 : 1.11 V 111 : 1.20 V Reported voltage values are nominal values at low-lane rates with de-emphasis disabled |
||
| [3] | Reserved | Read or write | 0 | Reserved and must be written as 0. | ||
| [2:0] | DEM[2:0] | Read or write | 000 | Serial lane transmitted de-emphasis. De-emphasis value are for VOD configured to 100. |
||
| DEM | De-emphasis [dB] | |||||
| 000 | 0.0 | |||||
| 001 | 1.4 | |||||
| 010 | 3.4 | |||||
| 011 | 4.9 | |||||
| 100 | 5.9 | |||||
| 101 | 7.4 | |||||
| 110 | 8.9 | |||||
| 111 | 12.1 | |||||
| Note: Before altering any parameters in this register, one must set JESD_EN = 0. Changing parameters while JESD_EN = 1 is not supported. | |||||
|---|---|---|---|---|---|
| Bit | Field | Type | Reset | Description | |
| [7] | SCR_EN | Read or write | 0 | Scrambler enable. 0 : Disabled (default) 1 : Enabled Note:
|
|
| [6:2] | K_M1[4:0] | Read or write | 11111 | Number of frames per multi-frame, K – 1. The binary values of K_M1 represent the value (K – 1) 00000 : Reserved 00001 : Reserved … 00111 : Reserved 01000 : K = 9 … 11111 : K = 32 (default) Note:
|
|
| [1] | Reserved | Read or write | 0 | Reserved and must be written as 0. | |
| [0] | JESD_EN | Read or write | 1 | JESD204B link enable. When enabled, the JESD204B link synchronizes and transfers data normally. When the link is disabled, the serial transmitters output a repeating, alternating 01010101 stream. 0 : Disabled 1 : Enabled (default) |
|
| Note: Before altering any parameters in this register, one must set JESD_EN = 0. Changing parameters while JESD_EN = 1 is not supported. | |||||
|---|---|---|---|---|---|
| Bit | Field | Type | Reset | Description | |
| [7] | SYNC_SEL | Read or write | 0 | SYNCb Signal MUX Select 0 : The internal SYNCb signal is routed from the SYNCb+/- pins (default) 1 : The internal SYNCb signal is routed from the JSYNC_N register field (SYNCb over SPI) |
|
| [6] | JSYNC_N | Read or write | 0 | SYNCb Over SPI Control 0 : The internal SYNCb signal as asserted, indicating a JESD204 link synchronization request (default) 1 : The internal SYNCb signal is de-asserted, indicating JESD204 link synchronization is not being requested Note: JSYNC_N controls the internal SYNCb signal only when SYNC_SEL = 1. When SYNC_SEL = 0, this register field is ignored. |
|
| [7:4] | Reserved | Read or write | 00 | Reserved. Must be written as 00. | |
| [3:0] | JESD_TEST_MODES[3:0] | Read or write | 0000 | JESD204B test modes. 0000 : Test mode disabled. Normal operation (default) 0001 : PRBS7 test mode 0010 : PRBS15 test mode 0011 : PRBS23 test mode 0100 : RESERVED 0101 : ILA test mode 0110 : Ramp test mode 0111 : K28.5 test mode 1000 : D21.5 test mode 1001: Logic low test mode (serial outputs held low) 1010: Logic high test mode (serial outputs held high) 1011 – 1111 : Reserved Note:
|
|
| Bit | Field | Type | Reset | Description | |
|---|---|---|---|---|---|
| 0x0062[7:0] | JESD_RSTEP [7:0] |
Read or write | 0x01 | JESD204B ramp test mode step | |
| 0x0063[7:0] | JESD_RSTEP [15:8] |
Read or write | 0x00 | The binary value JESD_RSTEP[15:0] corresponds to the step of the ramp mode step. A value of 0x0000 is not allowed. Note:
|
|
| Bit | Field | Type | Reset | Description | |
|---|---|---|---|---|---|
| [7] | Reserved | Read | N/A | Reserved. | |
| [6] | LINK | Read | N/A | JESD204B link status This bit is set when synchronization is finished, transmission of the ILA sequence is complete, and valid data is being transmitted. 0 : Link not established 1 : Link established and valid data transmitted |
|
| [5] | SYNC | Read | N/A | JESD204B link synchronization request status This bit is cleared when a synchronization request is received at the SYNCb input. 0 : Synchronization request received at the SYNCb input and synchronization is in progress 1 : Synchronization not requested Note:
|
|
| [4] | REALIGN | Read or write | N/A | SYSREF re-alignment status This bit is set when a SYSREF event causes a shift in the phase of the internal frame or LMFC clocks. Note:
|
|
| [3] | ALIGN | Read or write | N/A | SYSREF alignment status This bit is set when the ADC has processed a SYSREF event and indicates that the local frame and multi-frame clocks are now based on a SYSREF event. Note:
|
|
| [2] | PLL_LOCK | Read | N/A | PLL lock status. This bit is set when the PLL has achieved lock. 0 : PLL unlocked 1 : PLL locked |
|
| [1] | CAL_DONE | Read | N/A | ADC calibration status This bit is set when the ADC calibration is complete. 0 : Calibration currently in progress or not yet completed 1 : Calibration complete Note:
|
|
| [0] | CLK_RDY | Read | N/A | Input clock status This bit is set when the ADC is powered-up and detects an active clock signal at the CLKIN input. 0 : CLKIN not detected 1 : CLKIN detected |
|