SNVA406C May   2010  – January 2022 LM27402

 

  1.   1
  2.   2
  3.   3
  4.   4
  5.   5
  6.   6
  7.   7
  8.   8
  9.   9
  10.   10
    1.     11
    2.     12
    3.     13
    4.     14
    5.     15
    6.     16
    7.     17
    8.     18
    9.     19
    10.     20
    11.     21
    12.     22
  11.   23
  12.   24
  13.   25

Input Capacitors, Cin1–Cin5

Input capacitors should be selected based on the required input voltage ripple and maximum RMS current rating. The required RMS current rating of the input capacitor for a buck regulator can be estimated by the following equation:

Equation 2. GUID-A87C92C9-5ADD-486E-801E-1C7D595C4549-low.gif

From this equation, it follows that the maximum ICIN(RMS) requirement will occur at a full 20-A load current with the system operating at 50% duty cycle. Under this condition, the maximum ICIN(RMS) is given by:

Equation 3. GUID-99781077-22B1-4C44-A7AC-4789ED621ED7-low.gif

The voltage ripple can be calculated by:

Equation 4. GUID-4B81D914-E9B0-43B2-A453-8443F36F7845-low.gif

Ceramic capacitors feature a very large IRMS rating in a small footprint, making a ceramic capacitor ideal for this application. Five 22-µF X5R 25-V ceramic capacitors were selected to provide the necessary input capacitance for the evaluation board. Neglecting the effects of ESR, at 12-V VIN and 20-A IOUT the selected input capacitors yield an input voltage ripple of:

Equation 5. GUID-2140EBE0-9255-49F2-923D-F76FC445B004-low.gif

If desired, two extra capacitors can be added in the Cin6 and Cin7 footprints.