ZHCSFI3B August 2016 – May 2019 UCD90320
PRODUCTION DATA.
The UCD90320 device is available in a 169-pin BGA package. If the design calls for the device to be mounted on the top layer, decoupling capacitors can be placed on the bottom layer to allow room for top-layer trace routing. The layout example below describes this strategy. Figure 43 shows bottom-layer component placement from top-view. In addition to Figure 43, consider these important suggestions.
Figure 43 shows a typical application with the UCD90320 device mounted on the top layer and the components placed on the bottom layer.