ZHCSIS2B september 2018 – december 2020 TPS7A11
PRODUCTION DATA
PIN | I/O | DESCRIPTION | |
---|---|---|---|
NAME | NO. | ||
IN | 6 | Input | Input pin. A capacitor is required from IN to ground for stability. For best transient response, use the nominal recommended value or larger ceramic capacitor from IN to ground. Follow the recommended capacitor value as listed in the Recommended Operating Conditions table. Place the input capacitor as close to the input pin of the device as possible. |
OUT | 1 | Output | Regulated output pin. A capacitor is required from OUT to ground for stability. For best transient response, use the nominal recommended value or larger ceramic capacitor from OUT to ground. Follow the recommended capacitor value as listed in the Recommended Operating Conditions table. Place the output capacitor as close to the output pin of the device as possible. |
GND | 5 | — | Ground pin. This pin must be connected to ground. |
BIAS | 4 | Input | BIAS pin. This pin enables the use of low-input voltage, low-output voltage (LILO) conditions. For best performance, use the nominal recommended value or larger ceramic capacitor from BIAS to ground. Follow the recommended capacitor value as listed in the Recommended Operating Conditions table. Place the bias capacitor as close to the bias pin of the device as possible. |
EN | 3 | Input | Enable pin. Driving this pin to logic high enables the device. Driving this pin to logic low disables the device. If enable functionality is not required, this pin must be connected to IN or BIAS; however, connecting EN to IN is only acceptable if the IN pin voltage is greater than 0.9 V. |
NC | 2 | — | This pin is not internally connected. Connect to ground for better thermal dissipation or leave floating. |
Thermal pad | — | Connect the thermal pad to a large-area ground plane. |
PIN | I/O | DESCRIPTION | |
---|---|---|---|
NO. | NAME | ||
A1 | IN | Input | Input pin. A capacitor is required from IN to ground for stability. For best transient response, use the nominal recommended value or larger ceramic capacitor from IN to ground. Follow the recommended capacitor value as listed in the Recommended Operating Conditions table. Place the input capacitor as close to the input pin of the device as possible. |
A3 | OUT | Output | Regulated output pin. A capacitor is required from OUT to ground for stability. For best transient response, use the nominal recommended value or larger ceramic capacitor from OUT to ground. Follow the recommended capacitor value as listed in the Recommended Operating Conditions table. Place the output capacitor as close to the output pin of the device as possible. |
B2 | GND | — | Ground pin. This pin must be connected to ground. |
C1 | BIAS | Input | BIAS pin. This pin enables the use of low-input voltage, low-output voltage (LILO) conditions. For best performance, use the nominal recommended value or larger ceramic capacitor from BIAS to ground. Follow the recommended capacitor value as listed in the Recommended Operating Conditions table. Place the bias capacitor as close to the bias pin of the device as possible. |
C3 | EN | Input | Enable pin. Driving this pin to logic high enables the device. Driving this pin to logic low disables the device. If enable functionality is not required, this pin must be connected to IN or BIAS; however, connecting EN to IN is only acceptable if the IN pin voltage is greater than 0.9 V. |