ZHCSGV1C June 2017 – March 2018 TPS25740B
PRODUCTION DATA.
An example of the BMC signal, specifically the end of the preamble and beginning of start-of-packet (SOP) is shown below. There is always an edge at the end of each bit or unit interval, and ones have an edge half way through the unit interval.
While engaging in USB PD communications, the device is applying I(RP1.5) or I(RP3.0), so the CC line has a DC voltage of 0.918 V or 1.68 V, respectively. When the BMC signal is transmitted on the CC line, the transmitter overrides this DC voltage as shown in Figure 25. The transmitter bias rail (VTX) is internally generated and may not be used for any other purpose in the system. The VTX pin is only high while the TPS25740B is transmitting a USB PD message.
The device transmissions meet the eye diagram USB PD requirements (refer to USB PD in 文档支持) across the recommended temperature range. Figure 26 shows the transmitter schematic.
The transmit eye diagram shown in Figure 28 was measured using the test load shown in Figure 27 with a CLOAD within the allowed range. The total capacitance CLOAD is computed as:
Where:
Therefore, 400 pF < CLOAD < 1850 pF.
Figure 28 shows the transmit eye diagram for the TPS25740B.