SBOSAF3 November 2023 TMCS1126
ADVANCE INFORMATION
The ideal first-order transfer function of the TMCS1126 is given by Equation 1, where the output voltage is a linear function of input current. The accuracy of the device is quantified both by the error terms in the transfer function parameters, as well as by nonidealities that introduce additional error terms not in the simplified linear model. See Total Error Calculation Examples for example calculations of total error, including all device error terms.
where