ZHCSHZ4D April 2018 – October 2023 TLV758P
PRODUCTION DATA
As with most LDOs, excessive reverse current can damage this device.
Reverse current flows through the body diode on the pass transistor instead of the normal conducting channel. At high magnitudes, this current flow degrades the long-term reliability of the device, as a result of one of the following conditions:
Conditions where reverse current can occur are outlined in this section, all of which can exceed the absolute maximum rating of VOUT > VIN + 0.3 V:
If reverse current flow is expected in the application, external protection must be used to protect the device. Figure 7-4 shows one approach of protecting the device.