ZHCU623 January 2019
The design has an embedded firmware that must be programmed to the patch. To compile and load the embedded firmware, the following software is required:
To view the temperature from the patch or connect to the patch, the following application is required on an iOS-enabled smartphone or tablet.