ZHCSFV6E august 2016 – november 2020 DS90UB933-Q1
PRODUCTION DATA
The DS90UB933/934/964 chipsets can be operated by using the pixel clock from the imager as the reference clock. Figure 7-5 shows the operation of the DS90UB933/934/964 chipsets using the pixel clock from the imager. If the DS90UB933-Q1 device is operated using the pixel clock from the imager as the reference clock, then the imager uses an external oscillator as its reference clock. There are 4 GPIOs available in this mode (PCLK from imager mode).
Figure 7-5 DS90UB933-Q1/934-Q1 Operation in PCLK mode