TIDUES0F June 2019 – April 2026 TMS320F28P550SG , TMS320F28P550SJ , TMS320F28P559SG-Q1 , TMS320F28P559SJ-Q1
In this setup, the DC source is connected to the secondary side and the resistive load is connected to the primary side.
Compile the project by selecting Lab 5: Open Loop PWM, Sec to Prim Power Flow in the drop-down menu of Project Options from PowerSUITE GUI. Make sure current and voltage limits are set per operating conditions.
#if DAB_LAB == 5
#define DAB_CONTROL_RUNNING_ON C28X_CORE
#define DAB_POWER_FLOW DAB_POWER_FLOW_SEC_PRI
#define DAB_INCR_BUILD DAB_OPEN_LOOP_BUILD
#define DAB_CONTROL_MODE DAB_VOLTAGE_MODE
#define DAB_TEST_SETUP DAB_TEST_SETUP_RES_LOAD
#define DAB_PROTECTION DAB_PROTECTION_ENABLED
#define DAB_SFRA_TYPE 2
#define DAB_SFRA_AMPLITUDE (float32_t)DAB_SFRA_INJECTION_AMPLITUDE_LEVEL2
#endifsetupdebugenv_lab5.js
in the scripting console.
Figure 4-41 Lab 5 - Watch
ViewDAB_enableFan and
DAB_enableRelay.DAB_clearTrip variable.DAB_pwmPhaseShiftPrimSec_pu and
observe the change in voltage at the output of converter.
Figure 4-42 Lab 5 - Primary Side
Overvoltage Protection
Figure 4-43 Lab 5 Expression
Window High Voltage