TIDT369A November 2023 – April 2024
A MOSFET, as shown in Figure 2-1, is used as a solid-state relay (SSR) in this design. The SSR provides faster response time, wider operational temperature range, higher reliability than the traditional mechanical relay. Moreover, M-CRPS requires input current (re-rush current) must be limited when the input voltage returns after an input brown out / black out event for a few ms. Due to the fast response time, the SSR is controlled to do a rapid on/off operation to limit the re-rush currrent. Details of re-rush control can be found in [1][2].