SWRZ098 April 2021 AWR6443
Second Harmonic (HD2) Present in the Receiver
AWR6443 ES2.0
There is a finite isolation between the RF pins/package and the FMCW synthesizer. This can create spurious tones at the synthesizer output and lead to appearance of 2nd order harmonics and inter-modulations of expected IF frequencies at RX ADC output. The amplitude of the 2nd harmonic could be as high as -55 dBc , referenced to the power level of the intended tone at the LNA input.
No workaround available at this time. However, in many typical radar use-cases the HD2 does not affect the system performance due to two reasons: