SWRU455M February 2017 – October 2020 CC3120 , CC3120MOD , CC3130 , CC3135 , CC3135MOD , CC3220MOD , CC3220MODA , CC3220R , CC3220S , CC3220SF , CC3230S , CC3230SF , CC3235MODAS , CC3235MODASF , CC3235MODS , CC3235MODSF , CC3235S , CC3235SF
In this topology, only the RX, TX, and CTS lines are required. In this mode, the host is always able to receive any amount of data transmitted by the SimpleLink device because there is no flow control in this direction. Using this topology is allowed only if one of the following conditions is met:
Figure 24-14 3-Wire UART ConfigurationBecause there is no full flow control, the host cannot stop the SimpleLink device to send its data; thus, the following parameters must be considered: