SWRU271I October 2010 – January 2020 CC2540 , CC2540T , CC2541 , CC2541-Q1 , CC2640R2F
To open an existing project when using Windows, do the following:
For the required version of IAR, refer to the SDK release notes.
When IAR opens up, do the following:
This file is the workspace for the SimpleBLEPeripheral project. When you select this file, the files associated with the workspace should also open with a list of files on the left side. For the IAR Embedded Workbench, see Figure 8-1.
Figure 8-1 IAR Embedded Workbench