SWRA748 August 2022 CC2651R3SIPA
This device is intended for OEM integrators under the following conditions:
To comply with FCC / IC regulations limiting both maximum RF output power and human exposure to RF radiation, the maximum antenna gain including cable loss in a mobile exposure condition must not exceed:
In the event that these conditions cannot be met (for example certain laptop configurations or co-location with another transmitter), then the FCC / IC authorization is no longer considered valid and the FCC / IC ID cannot be used on the final product. In these circumstances, the OEM integrator will be responsible for re-evaluating the end product (including the transmitter) and obtaining a separate FCC / IC authorization.