SWRA733 March   2022 WL1807MOD , WL1837MOD

 

  1.   Trademarks
  2.   Acronyms
  3. 1Introduction
  4. 2 Single-Channel Versus Multi-Channel
    1. 2.1 MRSC Single Radio Network Topology
    2. 2.2 MRMC Single Radio Network Topology
    3. 2.3 Experiment and Results
  5. 3Multi-Channel Challenges and Requirements
    1. 3.1 802.11 Spec Enablers for Role Switch Protections
    2. 3.2 Role Switch Protection Implementations
      1. 3.2.1 AP Based Roles
      2. 3.2.2 STA Based Roles
    3. 3.3 Single Radio Multi-Channel Challenges
    4. 3.4 Single Radio Multi-Channel Key Requirements
  6. 4WL18xx™ Multi-Channel Implementations
    1. 4.1 Arranging the Role Activity Requests by Priority
    2. 4.2 Scheduling the Role Activities
    3. 4.3 Leveraging MRMC to Improve WLAN-BT Coexistence
  7. 5Conclusions
  8.   Appendix

MRMC Single Radio Network Topology

The following example will demonstrate the Multi-Role Multi-Channel use case and how system efficiency is significantly improved when roles are operating on different channels or bands. As can be seen in the Figure 2-2 below, the traffic does not overlap and no collisions between the IoT STAs connected to the Multi-Role device Access Point (“Red network”) and the Remote Station connected to the Remote Access Point (“Blue network”). Thus, overall system throughput is higher (very important for heavy data consumers). In addition, the system’s overall power consumption is lower as the amount of re-transmissions required from all the devices is lower compared to a single channel (very important for IoT nodes).

GUID-20220120-SS0I-XFCN-RZBT-KLHTG3KQJRVM-low.jpgFigure 2-2 Multi-Role Multi-Channel Network Topology