SWRA733 March   2022 WL1807MOD , WL1837MOD

 

  1.   Trademarks
  2.   Acronyms
  3. 1Introduction
  4. 2 Single-Channel Versus Multi-Channel
    1. 2.1 MRSC Single Radio Network Topology
    2. 2.2 MRMC Single Radio Network Topology
    3. 2.3 Experiment and Results
  5. 3Multi-Channel Challenges and Requirements
    1. 3.1 802.11 Spec Enablers for Role Switch Protections
    2. 3.2 Role Switch Protection Implementations
      1. 3.2.1 AP Based Roles
      2. 3.2.2 STA Based Roles
    3. 3.3 Single Radio Multi-Channel Challenges
    4. 3.4 Single Radio Multi-Channel Key Requirements
  6. 4WL18xx™ Multi-Channel Implementations
    1. 4.1 Arranging the Role Activity Requests by Priority
    2. 4.2 Scheduling the Role Activities
    3. 4.3 Leveraging MRMC to Improve WLAN-BT Coexistence
  7. 5Conclusions
  8.   Appendix

Experiment and Results

The test below compares the overall system efficiency (throughput) of a multi-role single-channel solution where both of STA and AP roles are running on the same channel as the external AP network versus a multi-role multi-channel solution where the AP role is running on a different band than the STA role and the external AP network. Please refer to the Appendix for the test setup details. See Figure 2-3 for a diagram of the test setup.

GUID-20220120-SS0I-FT1W-3NFJ-JMGTQD2FCTW6-low.jpgFigure 2-3 Test Setup Diagram

In the multi-role single-channel case the traffic running in the Multi-Role as an AP network (red network) impacts the traffic running in the External AP network where the External STA is also connected (blue network) and vice versa.

In the multi-role multi-channel case, the Multi-Role as an AP is operating on a different channel (and band) compared to the External AP. This actually creates a full separation between the two networks. It means that the traffic running in the Multi-Role as an AP network (red network) does not impacts the traffic running in the External AP network (blue network) and vice versa.

The test was repeated with increasing number of remote STAs from 1 to 5. The external STA was configured to send UDP of 50 Mbps while each Remote STA was configured to send UDP of 1 Mbps. For multi-channel versus single-channel results, refer to Table 2-1

The throughput results of this comparison are summarized in Table 2-2 and Figure 2-4.

Table 2-1 Multi-Channel Versus Single-Channel Results
Configuration Blue Network Red Network
Test Case Multi-Role AP (Red Network)

External AP

(Blue Network)

Bandwidth External STA Multi-Role STA Remote STA#1 Remote STA#2 Remote STA#3 Remote STA#4 Remote STA#5
Band CH Band CH
MRSC 2.4 GHz 11 2.4 GHz 11 SISO20 27.6 Mbps 1 Mbps 1.0 Mbps
MRMC 5 GHz 36 2.4 GHz 11 SISO20 27.8 Mbps 1 Mbps 1.0 Mbps
MRSC 2.4 GHz 11 2.4 GHz 11 SISO20 24.8 Mbps 2 Mbps 1.0 Mbps 1.0 Mbps
MRMC 5 GHz 36 2.4 GHz 11 SISO20 27.9 Mbps 2 Mbps 1.0 Mbps 1.0 Mbps
MRSC 2.4 GHz 11 2.4 GHz 11 SISO20 22.2 Mbps 3 Mbps 1.0 Mbps 1.0 Mbps 1.0 Mbps
MRMC 5 GHz 36 2.4 GHz 11 SISO20 27.5 Mbps 3 Mbps 1.0 Mbps 1.0 Mbps 1.0 Mbps
MRSC 2.4 GHz 11 2.4 GHz 11 SISO20 18.6 Mbps 4 Mbps 1.0 Mbps 1.0 Mbps 1.0 Mbps 1.0 Mbps
MRMC 5 GHz 36 2.4 GHz 11 SISO20 26.0 Mbps 4 Mbps 1.0 Mbps 1.0 Mbps 1.0 Mbps 1.0 Mbps
MRSC 2.4 GHz 11 2.4 GHz 11 SISO20 11.3 Mbps 4.6 Mbps 1.0 Mbps 1.0 Mbps 1.0 Mbps 0.6 Mbps 1.0 Mbps
MRMC 5 GHz 36 2.4 GHz 11 SISO20 24.7 Mbps 5 Mbps 1.0 Mbps 1.0 Mbps 1.0 Mbps 1.0 Mbps 1.0 Mbps
Table 2-2 Multi-Channel Throughput Improvement
Number of remote STAs

External STA throughput in

Single-Channel

External STA throughput

Multi-Channel

Improvement
127.6 Mbps27.8 Mbps0.7%
224.8 Mbps27.9 Mbps12.5%
322.2 Mbps27.5 Mbps23.87%
418.6 Mbps26.0 Mbps39.78%
511.3 Mbps24.7 Mbps118.58%
GUID-20220120-SS0I-R31Q-JFCB-RLFCZCSBC8CT-low.jpgFigure 2-4 Multi-Channel Throughput Improvement

As can be seen from the results, when each network was operating on a different channel and band (multi-channel) the overall throughput of the external STA was better for any number of remote STAs used. The throughput improvement is significantly higher when number of remote STAs in increased and can get to more than 100% with 5 remote STAs. This is directly related to the networks separation between bands which helped to avoid the interference between the Remote STAs and the External STA even though they were not connected to the same access point.