SPRZ536A september   2022  – june 2023 AM69 , AM69A , TDA4AH-Q1 , TDA4AP-Q1 , TDA4VH-Q1 , TDA4VP-Q1

 

  1.   1
  2. 1Modules Affected
  3. 2Nomenclature, Package Symbolization, and Revision Identification
    1. 2.1 Device and Development-Support Tool Nomenclature
    2. 2.2 Devices Supported
    3. 2.3 Package Symbolization and Revision Identification
  4. 3Silicon Revision 1.0 Usage Notes and Advisories
    1. 3.1 Silicon Revision 1.0 Usage Notes
      1.      i2134
    2. 3.2 Silicon Revision 1.0 Advisories
      1.      i2049
      2.      i2062
      3.      i2063
      4.      i2064
      5.      i2065
      6.      i2079
      7.      i2097
      8.      i2102
      9.      i2120
      10.      i2134
      11.      i2137
      12.      i2146
      13.      i2157
      14.      i2159
      15.      i2160
      16.      i2161
      17.      i2163
      18.      i2166
      19.      i2177
      20.      i2189
      21.      i2190
      22.      i2196
      23.      i2197
      24.      i2205
      25.      i2215
      26.      i2216
      27.      i2219
      28.      i2232
      29.      i2234
      30.      i2242
      31.      i2244
      32.      i2245
      33.      i2249
      34.      i2253
      35.      i2271
      36.      i2272
      37.      i2278
      38.      i2279
      39.      i2310
      40.      i2311
      41.      i2312
      42.      i2320
      43.      i2326
      44.      i2351
      45.      i2362
      46.      i2366
      47.      i2371
      48.      i2372
      49.      i2378
      50.      i2381
      51.      i2383
  5.   Trademarks
  6.   Revision History

i2378

MSMC: Cache/snoop filter way selection MMRs have incorrect reset values

Details:

The shadow copies of the following two MSMC MMRs have the wrong reset value. The main copy that SW can read have the correct reset value, but MSMC functionality uses the value in the shadow copies. The incorrect reset values results in reduced DDR system performance. More specifically MSMC L3 data cache and snoop filter to be under-utilized for DDR accesses (utilization drops to 25% of expectations). The under-utilization extends to the L2 cache of the A72 [include in J7AEP-only: "and C7x"].

RT_WAY_SELECT [Address = 0x6E00_8000]

NRT_WAY_SELECT [Address = 0x6E00_8008]

Workaround(s):

SW needs to write the value (0x0000_0303) to both MSMC MMRs after reset. This is needed even if the MMRs appear to already have the correct value. Writing to the MMRs ensure that their shadow copies have the correct post-reset value.