SPRUIG6J January 2018 – December 2023
The C7000 Host Emulation package generally allows
for the use of TI vector types (for example, int16
) to be used in
the same way as with the C7000 compiler. Boolean vectors, such as bool16, are also
supported.
However, due to C7000 Host Emulation being written in C++, there are limitations. The following sections discuss and provide examples of these limitations. Where limitations exist, usage and syntax changes may be required.