SPRU513AA July 2001 – March 2026 SM320F28335-EP
There are two rules to remember about the contents of output sections. An output section contains either:
A section that has raw data is referred to as initialized. This means that the object file contains the actual memory image contents of the section. When the section is loaded, this image is loaded into memory at the section's specified starting address. The .text and .data sections always have raw data if anything was assembled into them. Named sections defined with the .sect assembler directive also have raw data.
By default, the .ebss or .bss section and sections defined with the .usect directive (see Reserve Uninitialized Space) have no raw data (they are uninitialized). They occupy space in the memory map but have no actual contents. Uninitialized sections typically reserve space in fast external memory for variables. In the object file, an uninitialized section has a normal section header and can have symbols defined in it; no memory image, however, is stored in the section.