SPRAD65 December 2022 TDA4VM
This article takes 7.1SDK as an example to upgrade TIDL to version 8.4 and even though it is expected to work for other releases also but may need slight modification if you required. The upgrade methods for other versions are similar, and you can make your own if the upgraded version is the same as the version in the document, after copying the TIDL, MMALIB, and C7 compilers of 8.4SDK, you only need to use the two patch applications provided in the text to recompile the SDK. If the upgraded version is inconsistent with the text, you can refer to the steps in the text to generate the corresponding patch. It should be noted that after the upgrade, the previous version of the model cannot be run in the upgraded SDK, and the corresponding board model file must be re-imported.