SPRAD64 November   2022 AM620-Q1 , AM623 , AM625 , AM625-Q1

 

  1.   Trademarks
  2. 1 Introduction
  3. 2 Width/Spacing Proposal for Escapes
  4. 3 Stackup
  5. 4 Via Sharing
  6. 5 Floorplan Component Placement
  7. 6 Critical Interfaces Impact Placement
  8. 7 Routing Priority
  9. 8 SerDes Interfaces
  10. 9 DDR Interfaces
  11. 10Power Decoupling
  12. 11Route Lowest Priority Interfaces Last
  13. 12Summary

Power Decoupling

The middle priority interfaces and the power distribution planes and pours are routed next after the SerDes and DDR interfaces. TI recommends completing all SerDes and DDR routing before continuing with other interfaces. The power distribution planes and pours and all of the decoupling must be placed before PCB simulations are executed for the SerDes and DDR routes, as these can influence the return currents for the high-speed interfaces. The highest speed source-synchronous interfaces, such as RGMII and QSPI, may also require simulation thus these may also need to be completed at this time.

Special care is needed for the 1-uF output capacitors connected to the CAP_VDDS* BGA pins on the AM62x (AMC) device. These capacitors should be placed as close to the pin as possible and a low inductance path should be present between the CAP_VDDS BGA pin and the supply pad on the capacitor. The layout used on the CAP_VDDS1, CAP_VDDS3, and CAP_VDDS6 nets on the AM62x (AMC) board is shown below in Figure 10-1. The sharing of the GND pad of the capacitors is with other capacitors in the vicinity, which allows saving routing resources. Also, keep the PTH vias for the capacitor power and GND pad connections as close to each other as possible to minimize the loop inductance.

GUID-B3C41F04-731E-4063-9A1D-0390E67B21FD-low.png Figure 10-1 AM62 SK EVM Output Capacitor Placement for CAP_VDDS0

This placement can be improved if the capacitors are placed directly under the SoC. The decoupling capacitors for the VDD_CORE and VDDS_DDR supplies should also receive the same priority as those on the CAP_VDDS* pins and should be placed under the socket, with minimum inductance connections to the respective BGA pins on the AM62x (AMC) device.