SPRAD13 May   2022 AM623 , AM625

 

  1.   Abstract
  2.   Trademarks
  3. Introduction
  4. Via Channel Arrays
  5. Width/Spacing Proposal for Escapes
  6. Stackup
  7. Via Sharing
  8. Floorplan Component Placement
  9. Critical Interfaces Impact Placement
  10. Routing Priority
  11. SerDes Interfaces
  12. 10DDR Interfaces
  13. 11Power Decoupling
  14. 12Route Lowest Priority Interfaces Last
  15. 13Summary

Power Decoupling

The middle priority interfaces and the power distribution planes and pours are routed next after the SERDES and DDR interfaces. TI recommends completing all SERDES and DDR routing before continuing with other interfaces. The power distribution planes and pours and all of the decoupling must be placed before PCB simulations are executed for the SERDES and DDR routes, as these can influence the return currents for the high-speed interfaces. The highest speed source-synchronous interfaces, such as RGMII and QSPI, may also require simulation, thus these also may need to be completed at this time.

Special care is needed for the 1-uF output capacitors connected to the CAP_VDDS* BGA pins on the AM62 device. These capacitors should be placed as close to the pin as possible, and a low inductance path should be present between the CAP_VDDS BGA pin and the supply pad on the capacitor. The layout used on the CAP_VDDS0 net on the AM62 SK EVM is shown in Figure 11-1. Note the sharing of the GND pad of the capacitor with other capacitors in the vicinity, which allows saving routing resources. Also, keep the PTH vias for the capacitor power and GND pad connections as close to each other as possible to minimize the loop inductance.

GUID-20211214-SS0I-ZRNR-CQG9-RK2T6JKPSNNK-low.png Figure 11-1 AM62 SK EVM Output Capacitor Placement for CAP_VDDS0

This placement can be improved if the capacitors can be placed directly under the SoC. The decoupling capacitors for the VDD_CORE and VDDS_DDR supplies should also receive the same priority as those on the CAP_VDDS* pins, and should be placed under the socket, with minimum inductance connections to the respective BGA pins on the AM62 device.