SPNA243 June   2020 TM4C1236D5PM , TM4C1236D5PM , TM4C1236E6PM , TM4C1236E6PM , TM4C1236H6PM , TM4C1236H6PM , TM4C1237D5PM , TM4C1237D5PM , TM4C1237D5PZ , TM4C1237D5PZ , TM4C1237E6PM , TM4C1237E6PM , TM4C1237E6PZ , TM4C1237E6PZ , TM4C1237H6PGE , TM4C1237H6PGE , TM4C1237H6PM , TM4C1237H6PM , TM4C1237H6PZ , TM4C1237H6PZ , TM4C123FE6PM , TM4C123FE6PM , TM4C123FH6PM , TM4C123FH6PM , TM4C123GE6PM , TM4C123GE6PM , TM4C123GE6PZ , TM4C123GE6PZ , TM4C123GH6PGE , TM4C123GH6PGE , TM4C123GH6PM , TM4C123GH6PM , TM4C123GH6PZ , TM4C123GH6PZ , TM4C123GH6ZRB , TM4C123GH6ZRB , TM4C123GH6ZXR , TM4C123GH6ZXR

 

  1.   Using USB Host Mode on the EK-TM4C123GXL LaunchPad
    1.     Trademarks
    2. 1 EK-TM4C123GXL Board Overview
    3. 2 Board Modification to Make EK-TM4C123GXL USB Host/OTG Capable
    4. 3 Download and Import the USB Host Examples
    5. 4 Run the usb_host_mouse Example
      1. 4.1 Build and Flash the Program
      2. 4.2 Configure the Terminal Window
      3. 4.3 Run the usb_host_mouse Example
    6. 5 Run the usb_host_keyboard Example
    7. 6 Run the usb_stick_update and usb_stick_demo Examples
      1. 6.1 USB Memory Stick Updater (usb_stick_update) Overview
      2. 6.2 USB Stick Update Demo (usb_stick_demo) Overview
      3. 6.3 Add the FIRMWARE.BIN File in the Memory Stick
      4. 6.4 Run the usb_stick_update Program
      5. 6.5 Run the usb_stick_demo Program
    8. 7 References

Configure the Terminal Window

The example displays the status and coordinates of the mouse’s movements on the terminal window. You can use any terminal emulator of your choice. The terminal emulator should be configured for 115200 Baud and 8-N-1 as shown in Figure 10. For this document, the terminal emulator built into CCS will be used. You can launch the CCS terminal emulator by going to "View" → "Terminal".

Then select "Open a Terminal", and choose terminal type "Serial Terminal". Identify the COM Port for the LaunchPad "Stellaris Virtual Serial Port" and input that for the "Serial Port" entry and use the drop down menus to finish the configuration. This process will connect the terminal to the UART output that comes from the LaunchPad debug.

spna243-serial-terminal-settings.pngFigure 10. Serial Terminal Settings