SPMU420 April 2026 TPS65219
The TPS65219 allows to synchronize multiple devices in case more rails are required. The input functionality of the GPIO is only used in a multi-PMIC configuration. The configuration of the GPIO-pin is done writing to the MULTI_DEVICE_ENABLE bit in the MFP_1_CONFIG register. The table below shows the default multi-device register setting. For more information about the TPS65219 multi-PMIC operation, please refer to the device data sheet available on ti.com.
| Register Address | Field Name | Value | Description |
|---|---|---|---|
| 0x1F | MULTI_DEVICE_ENABLE | 0x0 | Single-device configuration, GPIO pin configured as GPO |