SPMA082 August 2021 TM4C1230C3PM , TM4C1230D5PM , TM4C1230E6PM , TM4C1230H6PM , TM4C1231C3PM , TM4C1231D5PM , TM4C1231D5PZ , TM4C1231E6PM , TM4C1231E6PZ , TM4C1231H6PGE , TM4C1231H6PM , TM4C1231H6PZ , TM4C1232C3PM , TM4C1232D5PM , TM4C1232E6PM , TM4C1232H6PM , TM4C1233C3PM , TM4C1233D5PM , TM4C1233D5PZ , TM4C1233E6PM , TM4C1233E6PZ , TM4C1233H6PGE , TM4C1233H6PM , TM4C1233H6PZ , TM4C1236D5PM , TM4C1236E6PM , TM4C1236H6PM , TM4C1237D5PM , TM4C1237D5PZ , TM4C1237E6PM , TM4C1237E6PZ , TM4C1237H6PGE , TM4C1237H6PM , TM4C1237H6PZ , TM4C123AE6PM , TM4C123AH6PM , TM4C123BE6PM , TM4C123BE6PZ , TM4C123BH6PGE , TM4C123BH6PM , TM4C123BH6PZ , TM4C123FE6PM , TM4C123FH6PM , TM4C123GE6PM , TM4C123GE6PZ , TM4C123GH6PGE , TM4C123GH6PM , TM4C123GH6PZ , TM4C1290NCPDT , TM4C1290NCZAD , TM4C1292NCPDT , TM4C1292NCZAD , TM4C1294KCPDT , TM4C1294NCPDT , TM4C1294NCZAD , TM4C1297NCZAD , TM4C1299KCZAD , TM4C1299NCZAD , TM4C129CNCPDT , TM4C129CNCZAD , TM4C129DNCPDT , TM4C129DNCZAD , TM4C129EKCPDT , TM4C129ENCPDT , TM4C129ENCZAD , TM4C129LNCZAD , TM4C129XKCZAD , TM4C129XNCZAD
void PixelDrawMultiple(void *pvDisplayData, long lX, long lY,
long lX0, long lCount, long lBPP,
const unsigned char *pucData,
const unsigned char *pucPalette);
The PixelDrawMultiple function is used when displaying images. A block of pixel data representing a given horizontal span is passed to the display driver, which renders the pixel data onto the display at the specified position. In this case, the driver must support 1 bpp, 4 bpp, and 8 bpp pixel formats. Displays supporting 16 bpp formats may also support native 16 bpp pixels.
For the 1 bpp pixel format, the pucPalette points to a 2-entry array containing pre-translated colors for background and foreground pixels. For 4 bpp and 8 bpp formats, the pucPalette parameter points to a color table containing RGB24 colors which the driver must translate to the native color format during the drawing process.
The palette is ignored for the 16 bpp formats since it is assumed that the pixels passed are in the native color format of the display.
When using 1 bpp and 4 bpp formats, the lX0 parameter indicates where the first pixel to draw is within the first byte of supplied pixel data. For 1 bpp, valid values are 0 through 7 and for 4 bpp, values 0 or 1 may be used. In each case, pixels are packed with the leftmost pixel in the most significant bit or nibble of the byte. Taking 1bpp as an example, if lX0 is 5 this indicates that the 5 leftmost pixels are skipped in the first byte passed and will draw 3 pixels from that byte. These will be taken from bits 2 , 1 and 0 of the byte.