SNVU834 September 2022
See Figure 1-2 for jumper locations.
J2 EN- This jumper allows the ENABLE input to be connected to GND in order to disable the IC. The "ON" position is the same as an unconnected jumper as EN is pulled up by R2. The "OFF" position shorts EN to ground which will disable TPSM365R6FRDNR.
Figure 1-2 Jumper Locations