SNVU834 September   2022 TPSM365R6

 

  1.   Abstract
  2.   Trademarks
  3. 1Setup
    1. 1.1 Test Points
    2. 1.2 Jumpers
  4. 2Operation
    1. 2.1 Quick Start
  5. 3Schematic
  6. 4Board Layout
  7. 5Bill of Materials
  8. 6Typical Characteristics
  9. 7Application Curves

Quick Start

  1. Make sure that a jumper is connected to one of the frequencies on the frequency select header. The device does not function properly if this is not connected.
  2. Connect the load between the VOUT and GND points on J4. Make sure GND is connected on the top terminal, and VOUT is located on the bottom terminal.
  3. Set the supply voltage at an appropriate level between 3.0 V to 65 V. Set the current limit of the supply to an appropriate level.
  4. Turn on the power supply. With the default configuration, the EVM powers up and provides VOUT = 5.0 V.
  5. Monitor the output voltage. The maximum load current is limited to 0.6 A with the TPSM36506 device.
  6. Connect the voltage supply between the VIN and GND points on J1.