SNIK006A April   2025  – June 2025 TMP9R01-SP

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1 Introduction
  5. 2 Sample Identification
  6. 3 Irradiation Facility and Setup
  7. 4 Die Micro-section
  8. 5 Test Set-Up
  9. 6 SEL Results
    1. 6.1 TMP9R01-SP SEL Data
  10. 7 SET Results
    1. 7.1 Summary of SET Results
      1. 7.1.1 Summary of SET Results Continued
    2. 7.2 Cross Section Events and Event Rate Calculations
  11. 8 Detailed Results Per Run
    1. 8.1 Detailed Run Raw Data
  12. 9 Summary
  13. 10Glossary
  14. 11Revision History

Irradiation Facility and Setup

The heavy-ion species used for the SEE studies on this product were provided and delivered by two facilities:

  • Michigan State University (MSU) Facility for Rare Isotope Beams (FRIB) using a linear accelerator and an advanced electron cyclotron resonance (ECR) ion source. At the fluxes used, ion beams had good flux stability and high irradiation uniformity as the beam is collimated to a maximum of 20mm x 20mm square cross-sectional area for the in-vacuum scintillator. Uniformity is achieved by scattering on a Cu foil and then performing magnetic defocusing. The flux of the beam is regulated over a broad range spanning several orders of magnitude. For these studies, ion flux of 9.36 x 104 to 1.07 x 105 ions/cm2 ·s was used to provide heavy-ion fluences of 1.00 x 107 ions/cm2.
  • Texas A&M University (TAMU) Cyclotron Radiation Effects Facility using a superconducting cyclotron and an advanced electron cyclotron resonance (ECR) ion source. At the fluxes used, ion beams had good flux stability and high irradiation uniformity over a 1-in diameter circular cross-sectional area for the in-air station. Uniformity is achieved by magnetic defocusing. The flux of the beam is regulated over a broad range spanning several orders of magnitude. For these studies, ion flux of 5.08 x 104 to 6.39 x 104 ions/cm2 ·s was used to provide heavy-ion fluences of 1.00 x 107 ions/cm2 .
Table 3-1 Ions and LETEFF Used for SEE Characterization
Ion TypeLocationAngle of IncidenceFLUX (ions·cm2/mg)FLUENCE (# ions)LETEFF (MeV-cm2/mg)

169Tm

MSU

0°

1.00 × 105

1.00 × 107

75

165Ho

TAMU

0°

1.00 × 1051.00 × 107

75.1

129Xe

MSU

0°

1.00 × 1051.00 × 107

50.5

84Kr

MSU

0°1.00 × 1041.00 × 106

35.4

40Ar

MSU

0°1.00 × 1041.00 × 106

7.9