SNAU267A June   2021  – June 2021

 

  1.   1
  2.   2
  3.   3
  4.   4
    1.     5
    2.     6
    3.     7
    4.     8
    5.     9
  5.   10
    1.     11
    2.     12
  6.   13
    1.     14
    2.     15
    3.     16
    4.     17
  7.   18
  8.   19
  9.   20
  10.   21

Home Tab

The Home tab is shown at software launch. The icons on the left side of the screen are shortcuts which can be used for navigation to other tabs within the GUI. They are identical to the icons on the bottom half of the Home page.

If the HDC3020EVM is connected to the PC and powered on, the Hardware Connected icon will appear on the left corner of the status bar.

GUID-20210610-CA0I-R6VN-RF9N-VPFGBB85TRVW-low.png Figure 5-1 Home Tab of the HDC3020EVM GUI