SLYA060 August   2022 TMAG5110 , TMAG5110-Q1 , TMAG5111 , TMAG5111-Q1

 

  1.   Abstract
  2.   Trademarks
  3. 1 Introduction
  4. 2 System Block Diagram
  5. 3 Key System Specifications
  6. 4 HW Connections
  7. 5 Software
    1. 5.1 TI-RSLK LaunchPad Software
    2. 5.2 LaunchPad Software
  8. 6 How to Design With Hall-Effect Latches
  9. 7 Simulation Results
    1. 7.1 Select Device Sensitivity
    2. 7.2 Select Axis of Sensitivity
  10. 8 Performance Comparison
    1. 8.1 Speed and Direction
    2. 8.2 Power Consumption
    3. 8.3 Susceptibility to External Particles
  11. 9 Encoder Board Schematic and Image
  12. 10Summary

Select Axis of Sensitivity

In rotary encoding systems that require both speed and direction, the sensors should be placed ideally 90° out of phase from each other. Using a 2D sensor enables the user to achieve this 90° offset more simply because the sensors are naturally orthogonal to each other, meaning there is a natural 90° phase difference from each sensor. This means that, when picking a 2D sensor, it is necessary to pick the two directions that have the closest phase angle difference of 90° from each other. To calculate this, we can use the following formula:

Equation 2. θ°=x2-x1period×360°

Where X2- X1 is the difference between the leading and lagging sinusoidal waveforms. This difference is converted to a fraction by dividing it by the entire period of the signals.

The fraction multiplied by 360° will provide the phase difference between the two sinusoidal waveforms. On the encoder board that was created, due to the rotation of the sensor (board image in Figure 9-2), a 65.45° offset was estimated from the simulation. The phase angle calculation is below.

Equation 3. 65.45°=25-1933×360°
With ideal Hall sensor placement, meaning a 90° angle is achieved, the signal should yield a 50% duty cycle on the output. When the offset is greater or lesser than 90°, it may lead to uneven periods in the duty cycle, as seen for this system in Figure 8-6.